Edit

OpenThread SDK Version 3.0.3 - Release Notes (Nov 4, 2026)#

OpenThread Version 3.0.3

Thread is a secure, reliable, scalable, and upgradeable wireless IPv6 mesh networking protocol. It provides low-cost bridging to other IP networks while optimized for low-power/battery-backed operation. The Thread stack is designed specifically for Connected Home applications where IP-based networking is desired and a variety of application layers may be required.

OpenThread, released by Google, is an open-source implementation of Thread. Google has released OpenThread to accelerate the development of products for the connected home and commercial buildings. With a narrow platform abstraction layer and a small memory footprint, OpenThread is highly portable. It supports system-on-chip (SoC), network co-processor (NCP), and radio co-processor (RCP) designs.

Silicon Labs has developed an OpenThread-based SDK tailored to work with Silicon Labs hardware. The Silicon Labs OpenThread SDK is a fully tested enhanced version of the GitHub source. It supports a broader range of hardware than does the GitHub version and includes documentation and example applications not available on GitHub.

Click here for earlier releases.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 3.0.3#

None.

Added in 3.0.2#

None.

Added in 3.0.1#

None.

Added in 3.0.0#

  • Continued compliance for Thread 1.4 on SoC and OTBR.

  • OpenThread Border Router in NCP mode with Thread 1.3 feature support.

  • Multi-PAN support for Thread in SoC mode.

API Changes#

Changed in 3.0.3#

None.

Changed in 3.0.2#

None.

Changed in 3.0.1#

None.

Changed in 3.0.0#

Refer to API changes as documented here, starting with the changes on May 23, 2025 and ending with the changes on November 11, 2025.

Bug Fixes#

Fixed in 3.0.3#

Targeted quality improvements and bug fixes.

Fixed in 3.0.2#

Targeted quality improvements and bug fixes.

Fixed in 3.0.1#

Targeted quality improvements and bug fixes.

Fixed in 3.0.0#

  • Added sample app board restrictions.

  • Studio Configuration Fixes.

  • Targeted quality improvements and bug fixes.

Chip Enablement#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 3.0.3#

None.

Added in 3.0.2#

None.

Added in 3.0.1#

None.

Added in 3.0.0#

Continued compliance for Thread 1.4 on SoC and OTBR#

Thread 1.4 specification introduces the following mandatory features for the Border Router:

  • Thread Credential Sharing

    • Provides a standard protocol to allow Administrator access to Thread Border Routers.

    • Enables authentication via a short one-time/ephemeral “Thread Administrator Passcode”.

  • Diagnostics: Network Management and Troubleshooting

    With Mesh devices having transient roles and being difficult to troubleshoot, this feature:

    • Enables enumeration of network participants and means to recreate network state at any time.

    • Disambiguates distinctions between various network layers.

    • Helps classify network diagnostic information for user purposes.

  • Thread over Infrastructure aka TREL

    • Allows Thread to utilize Wi-Fi/Ethernet links in the Thread mesh topology.

    • Enables merging of Thread Partitions over Wi-Fi/Ethernet.

  • Public Internet Connectivity IPv4 / IPv6 support

    DHCPv6 prefix delegation supports IPv6 prefix delegation and distribute prefixes in the interior network. Also enables DHCPv6-PD client support in the external IPv6 network.

  • Outbound IPv4 connectivity

    To support stateful NAT64 as a solution for IPv6/IPv4 translation.

  • DNS Recursive Resolver

    Allows subscriptions over TLS/TCP (where TCP is preferred over UDP because service lists can lead to quite large packets).

  • TCP (Bulk Transfer Protocol)

    Support for TCP as a standard component/protocol on Thread stacks to remedy throughput shortcomings for Bulk Transfer.

OpenThread Border Router in NCP mode with Thread 1.3 feature support#

This release adds Thread 1.3 support to the OpenThread Thread Border Router using the Network Co-Processor (NCP) architecture.

Multi-PAN support for Thread in SoC mode#

This release adds Multi-PAN (multi-instance) support for Thread in SoC mode to the OpenThread Platform Abstraction Layer (PAL). OpenThread typically supports only a single instance per device. Enabling multiple instances allows one device to participate in multiple independent Thread networks simultaneously. This is useful for applications that require network isolation or concurrent operation of separate Thread networks.

This feature is distinct from Multi-PAN RCP. In a Multi-PAN Radio Co-Processor (RCP) configuration, a host processor manages multiple IEEE 802.15.4 networks through a single RCP. The RCP does not maintain network state; it simply provides radio services for multiple networks managed by the host. This setup is often used to run a Zigbee and a Thread network concurrently. By contrast, in a multi-instance SoC application, multiple OpenThread stacks run directly on the SoC, allowing the device itself to join and operate in several independent Thread networks using its own local resources.

This release also includes three new sample applications that demonstrate multi-instance support:

  • ot-cli-ftd-multi-instance

  • ot-cli-mtd-multi-instance

  • ot-ble-dmp-multi-instance

These sample applications extend the existing ot-cli-ftd, ot-cli-mtd, and ot-ble-dmp applications by adding multi-instance support and the new multi-instance CLI component. This component enables you to switch between, control, and monitor individual Thread instances from a single command-line interface. You can:

  • List all active instances

  • Switch the CLI context to a specific instance

  • Perform instance-specific operations: attach, detach, form network, and more

Enhancements#

Added in 3.0.3#

None.

Added in 3.0.2#

None.

Added in 3.0.1#

  • Upgrade Rules

    A new upgrade rule was added that will automatically add CLI support to NCP applications.

  • TrustZone applications

    OpenThread TrustZone applications now utilize all available flash and RAM memory.

Added in 3.0.0#

  • Multi-instance support for OpenThread SoC apps

    Added support for multiple static OpenThread instances for SoC app configurations. The following sample apps were added to show the use of this multi-instance support: ot-cli-ftd-multi-instance, ot-cli-mtd-multi-instance, and ot-ble-dmp-multi-instance.

  • Reorganization of ot-ncp sample application folders

    The ot-ncp sample application variants have been reorganized into separate folders based on whether they require CPC or Bluetooth.

  • OPENTHREAD_CONFIG_MAC_STAY_AWAKE_BETWEEN_FRAGMENTS

    The OPENTHREAD_CONFIG_MAC_STAY_AWAKE_BETWEEN_FRAGMENTS option has been removed from certification configurations, as it can lead to sub-optimal power consumption for sleepy devices

  • Source match table size validation

    When the source match table in spinel on the host is larger than the source match tables on the RCP an error of "NoBufs" can be returned by the RCP after an RCP reset and during the restoration process of the source match table. This is because the host has more entries than the RCP tables can hold. To address this we now ensure the size of the RCP Source Match Table is large enough to support the maximum number of children for all interfaces on the host, including Zigbee in a multiprotocol environment.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

Changed in 3.0.3#

None.

Changed in 3.0.2#

None.

Changed in 3.0.1#

None.

Changed in 3.0.0#

Refer to API changes as documented here starting with the changes on May 23, 2025 and ending with the changes on November 11, 2025.

Bug Fixes#

Fixed in 3.0.3#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1636841, 1635295 Fixed a busfault / hardfault that could occur at runtime in OpenThread applications built with NDEBUG=1. 00341017 All OPNs, boards, modes and interfaces
1780572, 1758090 Fixed OTBR Debian package purge / reinstall behavior so leftover generated configuration files no longer trigger an interactive install prompt that blocks non-interactive OTBR installation. None Debian OTBR package installations
1787407, 1783696 Fixed an issue where Synchronized Sleepy End Devices (SSEDs), including the sleepy-demo-ssed sample, could lose parent synchronization after entering EM2. The first exchange after EM2 entry could succeed, but subsequent traffic failed until CSL timeout or a data poll triggered a full resync. None CSL Synchronized Sleepy End Devices (SSEDs), including sleepy-demo-ssed
1829676, 1824951 Fixed an issue where the coex metrics CLI command and otPlatRadioGetCoexMetrics() updated only the transmit and receive request counters. The other coexistence counters now update correctly. 00343966 Applications that use the coex metrics CLI command or the otPlatRadioGetCoexMetrics() API
1840390, 1839006 Fixed enhanced ACK Rx-to-Tx turnaround so that normal ACKs stay at 192 µs while CSL enhanced ACKs use 256 µs. Previously, the longer turnaround was applied to every ACK. 00333327 CSL configurations that use enhanced ACKs
1860223 Enforced KEK validation for Key ID Mode 0 frames. None Platforms that use key references

Fixed in 3.0.2#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1602474 During the join process for a Synchronized Sleepy End Device (SSED), the NCP support no longer errors out in the MAC when processing enhanced ACKs. This occurred only during the CSL negotiation and not in other cases. None Host / NCP architectures
1622614 In sisdk-2025.12.0 an issue was introduced where the CLI txpower command would return a value 10 times larger than the actual value. In sisdk-2025.12.3 this issue has been fixed and txpower now returns the correct value. 00340226 All OPNs, boards, modes and interfaces.

Fixed in 3.0.1#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1506512 Fixed an issue where OpenThread applications were experiencing sporadic failures when instruction cache (ICACHE) was disabled on SiXG301 devices. None SiXG301 devices
1566197 Fixed an issue where certain Thread communications could be disrupted between a pair of devices in which a ble connection is open. None SoC DMP architectures with BLE
1582133 Fixed issue in which the RTOS stack task would unexpectedly process serial data. None SiXG301 devices running OT+BLE DMP applications.
1589206 Fixed otPlatRadioEnergyScan to return OT_ERROR_BUSY when radio is already performing energy scan, as required by OpenThread platform API contract. None All OPNs, boards, modes and interfaces.
1590627 OTBR Debian packages now install NAT64 and other OTBR default services correctly. None Debian OTBR installations.
1605126 Fixed issue in which an assert is occasionally caused by starting an alarm while another alarm is active. 00335311 All OPNs, boards, modes and interfaces.

Fixed in 3.0.0#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1187748 Use the RAIL API RAIL_IEEE802154_SetRxToEnhAckTx to selectively set higher RxToTx for enhanced ACKs only. Previously, we were globally setting this higher RxToTx value for all ACKs. None All OPNs, boards, modes and interfaces
1415275, 1503788 Addressed a RAIL issue dealing with wraps of the microsecond timer. 00332010 All OPNs, boards, modes and interfaces
1475140 Addressed an issue where the txpower cli command would report the power as a negative number when the txpower was set at or above 13dBm. None All OPNs, boards, modes and interfaces
1476240 For Debian bookworm-based installations, when installing the ot-br-posix debian file, make sure the dhcpcd package on your target system is higher than the recommended bookworm version of 9.4.1-24, which has a known issue. The bookworm-backports apt source provides version 10.1.0 which is highly recommended. If not, we recommend updating your dhcpcd package version to at least 9.5.1. None Host processors using Debian packages
1491593 In Simplicity Studio, the rcp-spi-802154 and rcp-spi-802154-blehci sample apps are no longer available for boards chosen without a SPI capable external header. None Boards without a SPI capable external header
1499349 The OpenThread BLE DMP – SoC FreeRTOS (TrustZone) sample app should not show up as an available app for xGM270s modules and has been removed. None 270S Module
1507808 Fixed a hard fault which could occur when utilsSoftSrcMatchShortFindEntry was called with an invalid Iid. 00331602 All OPNs, boards, modes and interfaces
1511829 In Simplicity Studio, the sleepy_demo_ftd, sleepy_demo_mtd, and sleepy_demo_ssed sample apps are no longer available for boards that don't have at least 2 buttons. None Boards without 2 buttons
1560101 Addressed issues where configurable component options were not showing up correctly in the configuration editor in Simplicity Studio. None All OPNs, boards, modes and interfaces

Chip Enablement#

None.

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

Added in 3.0.3#

None.

Added in 3.0.2#

None.

Added in 3.0.1#

None.

Added in 3.0.0#

Example Name Description Supported Software Variants (if applicable) Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

ot-ncp-ftd-cpc

See README.

This is a simple OpenThread Full Thread Device NCP application with CPC. This is equivalent to the ot-ncp-ftd application in the OpenThread GitHub repo. Full Thread Device NCP All OPNs, boards, modes and interfaces All interfaces

ot-ncp-mtd-cpc

See README.

This is a simple OpenThread Minimal Thread Device NCP application. This is equivalent to the ot-ncp-mtd application in the OpenThread GitHub repo. Minimal Thread Device NCP All OPNs, boards, modes and interfaces All interfaces

ot-ble-dmp-multi-instance

See README.

This is a simple application to test DMP (Dynamic MultiProtocol) with OpenThread multi-instance and Bluetooth running on FreeRTOS. Full Thread Device, DMP, multi-instance SoC All OPNs, boards, modes and interfaces All interfaces

Modified Examples#

Modified in 3.0.3#

None.

Modified in 3.0.2#

None.

Modified in 3.0.1#

None.

Modified in 3.0.0#

  • The following CPC enabled sample apps have been moved from sample-apps/ot-ncp to sample-apps/ot-ncp/cpc

    • ot-ncp-ftd-cpc.slcp

    • ot-ncp-mtd-cpc.slcp

    • rcp-spi-802154.slcp

    • rcp-uart-802154.slcp

  • The following non-CPC enabled sample apps have been moved from sample-apps/ot-ncp to sample-apps/ot-ncp/ot

    • ot-ncp-ftd.slcp

    • ot-ncp-mtd.slcp

    • ot-rcp-spi.slcp

    • ot-rcp.slcp

  • The following BLE DMP enabled RCP sample apps have been moved from sample-apps/ot-ncp to sample-apps/ot-ncp/dmp

    • rcp-spi-802154-blehci.slcp

    • rcp-uart-802154-blehci.slcp

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

Issues in bold were added since the previous release.

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1559163 When running in a Host/NCP architecture and repeatedly sending factory resets to the NCP, after approximately 15 times the host will stop sending messages to the NCP. None The correct procedure when factory resetting the NCP is to also reset the host at the same time. Host / NCP architectures
1625968 Radio not idling when CSL is in use in multi-protocol environments. 00339903 Contact customer support for workaround. Multi-protocol environments with CSL enabled
1629296 RxFrame::ProcessReceiveAesCcm() takes 5ms to process on Series 2 platforms. 00340682 Contact customer support for workaround. All series 2 devices