Edit

Simplicity SDK Platform - Micrium OS Version 6.0.3 - Release Notes (Nov 4, 2026)#

Simplicity SDK Platform Version 6.0.3

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 6.0.1#

None.

Added in 6.0.0#

  • Restricted Micrium OS usage to Series 2 devices.

API Changes#

Changed in 6.0.1#

None.

Changed in 6.0.0#

None.

Bug Fixes#

Fixed in 6.0.2#

  • Fixed Studio configuration UI labels for BSP_LF_CLK_SEL and CPU_CFG_CACHE_MGMT_EN.

Fixed in 6.0.1#

  • Fixed OSTimeDly() overflow handling that could cause the delay to return immediately.

Fixed in 6.0.0#

None.

Chip Enablement#

Added in 6.0.1#

None.

Added in 6.0.0#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 6.0.1#

None.

Added in 6.0.0#

None.

Enhancements#

Added in 6.0.1#

None.

Added in 6.0.0#

Micrium OS: Usage is limited to Series 2 devices.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

None.

Modified APIs#

None.

Removed APIs#

None.

Deprecated APIs#

None.

Bug Fixes#

Fixed in 6.0.2#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
Configuration
1672985 Fixed the names of the options BSP_LF_CLK_SEL and CPU_CFG_CACHE_MGMT_EN in the Studio configuration UI. None Series 2 devices

Fixed in 6.0.1#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
RTOS
1596809 Fixed OSTimeDly() overflow handling that could cause the delay to return immediately; under periodic delays this could make TimeTask run continuously after extended uptime. None Series 2 Devices

Fixed in 6.0.0#

None.

Chip Enablement#

None.

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

None.

Modified Examples#

None.

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

None.