Edit

WiSeConnect - Wi-Fi SDK Version 4.0.3 (Jun 11, 2026) - Release Notes#

Wi-Fi 6 + BLE (WiSeConnect) SDK Version 4.0.3

Simplicity SDK Version 2025.12.3

The Wi-Fi Software Development Kit (SDK) provides Wi-Fi 6 connectivity in multiple operating modes, including Station and Software Access Point (SoftAP).

Click here for earlier releases.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 4.0.3#

None

Added in 4.0.2#

  • Enhanced background scanning (bgscan) to support extended scan results using a new advanced_scan_bitmap field in sl_wifi_advanced_scan_configuration_t, including a seen_count per AP and improved Beacon IE parsing with WPA/WPA2 mixed-mode detection.

Added in 4.0.1#

None

Added in 4.0.0#

  • Added Wi-Fi Protected Setup (WPS) Push Button Configuration (PBC) feature support in Station mode

  • Added Vendor-specific IE support for Station (STA), SoftAP, and Concurrent Modes

API Changes#

Added in 4.0.3#

None

Added in 4.0.2#

None

Added in 4.0.1#

None

Added in 4.0.0#

Bug Fixes#

Fixed in 4.0.3#

  • Fixed an issue where a TWT response could be observed on the host after the access point was power-cycled, even when no TWT API was invoked.

Fixed in 4.0.2#

  • Fixed an issue where the Wireless Test application became unresponsive when CLI commands (for example, wifi_ax_transmit_test_start) received more parameters than expected. Added parameter count validation to prevent this issue.

  • Fixed an issue that could cause the Wi-Fi mode set API to return error code -116 when configuring the device in SoftAP mode, ensuring reliable AP initialization across supported environments.

Fixed in 4.0.1#

  • Fixed a throughput drop in STA mode when 11w is enabled on the STA but disabled on the AP.

  • Fixed a DHCP handshake failure in Concurrent Mode with NAT+PAT enabled in congested environments.

Fixed in 4.0.0#

  • Fixed an issue where HTTP server encounters a connection timeout error when the web page is refreshed multiple times.

  • Added support for configurable PEAP security levels (PEAPSAFE1, PEAPSAFE2) through new encryption enum members to enhance enterprise Wi-Fi authentication security.

Chip Enablement#

Added in 4.0.3#

None

Added in 4.0.2#

  • Added support for BRD2708A board for the Wireless Test example (RF validation).

Added in 4.0.1#

None

Added in 4.0.0#

None

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces applicable for each feature.

New Features#

Added in 4.0.3#

None

Added in 4.0.2#

  • Added support for BRD2708A board for the Wireless Test example.

Added in 4.0.1#

None

Added in 4.0.0#

  • Added Wi-Fi Protected Setup (WPS) Push Button Configuration (PBC) feature support in Station mode

  • Added Vendor-specific IE support for Station (STA), SoftAP, and Concurrent Modes

  • An additional configurable option for Hidden SSID has been introduced in the sli_wifi_start_ap API, complementing the existing opermode configuration. The Hidden SSID can be configured via the sli_wifi_start_ap API only when SL_WIFI_CUSTOM_FEAT_AP_IN_HIDDEN_MODE is not enabled in custom_feature_bit_map.

  • Added support for reporting Wi-Fi band information for scanned access points in Wi-Fi scan results.

  • Improved SoftAP scan functionality to return more than 11 results.

Enhancements#

Added in 4.0.3#

None

Added in 4.0.2#

  • The keep-alive timer has been updated to reset only on actual data transmissions and not on Null or QoS-Null frames, thereby preventing indefinite GARP delays and improving interoperability.

  • The extended scan callback has been enhanced to report the required buffer size through the data_length parameter, enabling applications to dynamically allocate the exact amount of memory needed.

Added in 4.0.1#

None

Added in 4.0.0#

None

Removed Features#

Removed in 4.0.3#

None

Removed in 4.0.2#

None

Removed in 4.0.1#

None

Removed in 4.0.0#

None

Deprecated Features#

Deprecated in 4.0.3#

None

Deprecated in 4.0.2#

None

Deprecated in 4.0.1#

None

Deprecated in 4.0.0#

None

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 4.0.3#

None

Added in 4.0.2#

None

Added in 4.0.1#

None

Added in 4.0.0#

New API Signature

Deprecated API replaced by this (if any)

sl_status_t sl_wifi_get_interface_info (sl_wifi_interface_t interface, sl_wifi_interface_info_t *info)

sl_status_t sl_wifi_get_wireless_info (sl_si91x_rsp_wireless_info_t *info)

sl_status_t sl_wifi_set_scan_callback_v2 (sl_wifi_scan_callback_v2_t function, void *optional_arg)

sl_status_t sl_wifi_set_scan_callback (sl_wifi_scan_callback_t function, void *optional_arg)

sl_status_t sl_wifi_set_join_callback_v2 (sl_wifi_join_callback_v2_t function, void *optional_arg)

sl_status_t sl_wifi_set_join_callback (sl_wifi_join_callback_t function, void *optional_arg)

sl_status_t sl_wifi_set_twt_config_callback_v2 (sl_wifi_twt_config_callback_v2_t function, void *optional_arg)

sl_status_t sl_wifi_set_twt_config_callback (sl_wifi_twt_config_callback_t function, void *optional_arg)

sl_status_t sl_wifi_set_stats_callback_v2 (sl_wifi_stats_callback_v2_t function, void *optional_arg)

sl_status_t sl_wifi_set_stats_callback (sl_wifi_stats_callback_t function, void *optional_arg)

sl_status_t sl_wifi_set_transceiver_callback_v2 (sl_wifi_transceiver_callback_v2_t function, void *optional_arg)

sl_status_t sl_wifi_set_transceiver_callback (sl_wifi_transceiver_callback_t function, void *optional_arg)

sl_status_t sl_wifi_start_wps_v2 (sl_wifi_interface_t interface, sl_wifi_wps_config_t config, sl_wifi_wps_response_t *response)

sl_status_t sl_wifi_start_wps (sl_wifi_interface_t interface, sl_wifi_wps_mode_t mode, const sl_wifi_wps_pin_t *optional_wps_pin)

sl_status_t sl_wifi_get_saved_firmware_status (void)

sl_status_t sl_si91x_get_saved_firmware_status (void)

sl_status_t sli_net_register_event_handler (sli_net_event_handler_t handler, void *optional_arg)

sl_status_t sl_si91x_register_event_handler (sl_si91x_event_handler_t handler, void *optional_arg)

sl_status_t sli_net_set_credential (const sli_net_credential_t *credential)

sl_status_t sl_si91x_set_credential (const sl_si91x_credential_t *credential)

sl_status_t sli_net_get_credential (sl_net_credential_id_t credential_id, sli_net_credential_t *credential)

sl_status_t sl_si91x_get_credential (sl_si91x_credential_id_t credential_id, sl_si91x_credential_t *credential)

sl_status_t sli_net_delete_credential (sl_net_credential_id_t credential_id)

sl_status_t sl_si91x_delete_credential (sl_si91x_credential_id_t credential_id)

Modified APIs#

Modified in 4.0.3#

None

Modified in 4.0.2#

None

Modified in 4.0.1#

None

Modified in 4.0.0#

None

Removed APIs#

Removed in 4.0.3#

None

Removed in 4.0.2#

None

Removed in 4.0.1#

None

Removed in 4.0.0#

None

Deprecated APIs#

Deprecated in 4.0.3#

None

Deprecated in 4.0.2#

None

Deprecated in 4.0.1#

None

Deprecated in 4.0.0#

Deprecated API Name

Planned Removal Date

sl_wifi_get_wireless_info

2027-06

sl_wifi_set_scan_callback

2027-06

sl_wifi_set_join_callback

2027-06

sl_wifi_set_twt_config_callback

2027-06

sl_wifi_set_stats_callback

2027-06

sl_wifi_set_transceiver_callback

2027-06

sl_wifi_start_wps

2027-06

sl_si91x_get_saved_firmware_status

2027-06

sl_si91x_register_event_handler

2027-06

sl_si91x_set_credential

2027-06

sl_si91x_get_credential

2027-06

sl_si91x_delete_credential

2027-06

Bug Fixes#

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

Fixed in 4.0.3#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1651473 Fixed an issue where a TWT response could be observed on the host after the access point was power-cycled, even when no TWT API was invoked. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART

Fixed in 4.0.2#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1605946 Fixed an issue where the Wireless Test application became unresponsive when CLI commands (for example, wifi_ax_transmit_test_start) received more parameters than expected. Added parameter count validation to prevent this issue. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1615670 Fixed an issue that could cause the Wi-Fi mode set API to return error code -116 when configuring the device in SoftAP mode, ensuring reliable AP initialization across supported environments. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART

Fixed in 4.0.1#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1594590 Enhanced Wi-Fi extended scan functionality to accurately identify and report WPA3 Transition Mode access points. This addresses cases where extended scan may incorrectly display WPA2 security type instead of WPA3 Transition Mode, ensuring correct security information during provisioning and general scanning. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1581739 Enhanced Xmodem firmware upgrade example with improved initialization handling. This addresses cases where sl_net_init() returns SL_STATUS_ALREADY_EXISTS (0x002E) after firmware upgrade, ensuring smooth operation of the wifi_firmware_flashing_from_host_uart_xmodem_bootloader_ncp example. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1580084 Improved memory management in sli_si91x_wifi_event_handler.c by optimizing buffer lifecycle handling. This addresses use-after-free scenarios where buffer memory was accessed after being freed, which could lead to heap corruption and unstable RTOS behavior. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1578195 Improved buffer handling by initializing local pointer variables (buffer, packet, node, etc.) to NULL. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1574317 Added support for BRD2708A board for the Wireless Test example, expanding hardware compatibility for customer applications using this board. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1569213 Enhanced at+cal-start command handling in AT commands application. This addresses cases where the command may not execute as expected (error code 4) while maintaining proper M4 power save functionality. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1569000 Enhanced AT command parser and BSD socket commands with improved pointer handling and socket setup validation. This addresses TCP socket send API issues (error code 33) in at_commands application, improving reliability for AT command-based applications. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1559974 Enhanced sl_net_deinit() functionality with improved cleanup handling for auto-join operations. This addresses cases where sl_net_deinit() may fail with error 0x1 during multiple auto-join iterations, ensuring reliable behavior when switching between network profiles. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1533583 Enhanced flash_read_write example with data comparison verification for both TA and M4 regions. The update provides better validation of read/write operations and helps prevent data integrity issues during flash operations. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1576560 Updated the keep-alive timer so that it resets only on real data transmissions, but not on Null or QoS-Null frames, preventing indefinite GARP delays and interoperability issues. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1572862 Fixed a throughput drop in STA mode when 11w is enabled on the STA but disabled on the AP. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1557787 Fixed a DHCP handshake failure in Concurrent Mode with NAT+PAT enabled in congested environments. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART

Fixed in 4.0.0#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1465518 Fixed an issue where HTTP server encounters a connection timeout error when the webpage is refreshed multiple times. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1502308 Refactored socket allocation logic to use malloc/memset pattern with intermediate variable for improved error handling. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1522478 Improved async event processing and error handling. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1496506 The sl_net_init() API now returns an error if an attempt is made to modify the region code on modules where this operation is not permitted. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1365272 Added configurable timeout mechanism with scaling macros for management, internal, and network commands, plus additional wait time for buffer overflow and congestion scenarios. Defaults set to '1'. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1467697 Added support for Wi-Fi examples to the OPNs SIWG917Y121MGABA and SIWG917Y110LGABA None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1452673 Fixed a DTLS data transmission issue where packets could be lost if error 0x100D2 occurred, by implementing an automatic retry mechanism in the DTLS application with a default maximum of 3 retries. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1451080 Added the nvm3_lib component in the nvm3 config manager component instead of adding the nvm3_lib component for every application None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1407301 Azure IoT Hub and Device Provisioning Service (DPS) are migrating their certificate root of trust from the Baltimore CyberTrust Root (expiring in 2025) to the DigiCert Global Root G2. All devices must migrate from azure_baltimore_ca to silabs_digicert_ca for secure TLS connection with Azure IoT Hub and Azure storage services. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1409946 Added support for configurable PEAP security levels (PEAPSAFE1, PEAPSAFE2) through new encryption enum members for enhanced enterprise Wi-Fi authentication security. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1376228 Resolved firmware corruption during TLS socket cleanup post-IP change during DHCP renewal. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1371879 Updated sl_si91x_get_socket_info API to provide host socket info. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1268204 Deinitialize the Wi-Fi client interface when the power save profile is set to DEEP_SLEEP_WITHOUT_RAM_RETENTION. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1450227 SLI_MAX_RETRANSMISSION_TIME_VALUE has been updated to 255 (the maximum supported value) and can now be configured as a power of two from 1 to 128. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1441131 Replaced all breakpoints with the timeout indication recovery mechanism and with proper status. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1466129 Fixed static analysis issue by ensuring listen_interval is cast to uint16_t before assignment in the power save request struct. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1463798 Default configurations for Power Save Standby including NCP SoC and PSRAM are available when installing the Configuration Wizard. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1490559 The maximum client limit defined in the AP profile configuration will now automatically adjust if it exceeds the value set in the opermode configuration. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1426767 Replaced mixed BSD and sl-sockets with SiWx91x async sockets in sli_http_server(). None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1455876 Added configurable max retransmission timeout using AWS_IOT_MAX_RETRANSMISSION_TIMEOUT macro to avoid disconnection in case of AWS MQTT. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1464308 Resolved extended scan functionality by eliminating global variable dependency and ensuring controlled access. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1343541 Refactor the join configuration APIs from sl_si91x_ to sl_wifi_. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1467293 Resolved 'connection reset by peer' errors in RX scenarios for TCP, UDP, and TLS across all applications. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1464725 Added a conditional check to prevent setting WLAN_UNCONNECTED_STATE if the DUT is already connected. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1308081 For wlan throughput UART NCP applications, the handshake feature bit (SL_SI91X_FEAT_ULP_GPIO_BASED_HANDSHAKE) is enabled by default to ensure reliable socket connections and proper power save operation. You can control this feature using the SL_ENABLE_UART_NCP_BITMAP macro in your preprocessor settings. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1384564 Fixed callback status update order to maintain correct status in loop operation None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1478000 Added sl_string.h header file to provide proper declaration for sl_strnlen() function. Replaced standard strnlen() with SDK-specific sl_strnlen() implementation. Eliminates implicit declaration warnings and compilation failures. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1371872 Resolved the AzureIOT connection issue in the process loop by adding state machine checks. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1288559 Added the validation for client idle timeout in AP configuration and mentioned the note of its range and units. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1478082 Before each Wi-Fi scan, scan_complete and callback_status are now reset to ensure accurate results. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1513128 The default value of client_idle_timeout value is updated from 120000 to 255. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1385303 Added support for multiple network interface initialization tracking None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1455151 Fixed the network manager thread stack overflow during sl_net_deinit() by increasing default stack size to 3072 bytes and making it configurable via NETWORK_MANAGER_THREAD_STACK_SIZE. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1402599 To ensure the TA is also reset during an NCP reset, we are adding a call to sl_wifi_deinit() in the reset handler. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1467508 Wi-Fi initialization and deinitialization are managed only by the main application. This change prevents conflicts and ensures reliable operation during firmware updates. No impact to normal operation. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1321102 Adding continuous throughput for TCP RX and UDP RX in wifi_station_ble_throughput_app. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1407525 Replaced NVIC_SystemReset() with sl_si91x_soc_nvic_reset() in wireless test example for SoC None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: SPI, UART
1499542 Fix socket shutdown sequence for TCP server socket in the throughput test None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1511479 Restrict the module from setting the SL_SI91X_EXT_FEAT_FRONT_END_SWITCH_PINS_ULP_GPIO_4_5_0 bit. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1533724 Added certificate index for HTTPS GET/POST None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1515226 Replaced ACX module guard with internal antenna macro in sl_wifi_device.h None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1524218 Added error handling if any of the configuration is missed in the application. Enhanced MAX PSP is supported when the profile is set to ASSOCIATED_POWER_SAVE_LOW_LATENCY and SL_WIFI_ENABLE_ENHANCED_MAX_PSP bit is enabled in the config feature bitmap. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1449759 Added sl_http_server_init API checking if device is up or not. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1535260 For open security (SL_WIFI_OPEN), set credential_id to SL_WIFI_NO_CREDENTIAL_ID to avoid unnecessary credential fetch. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1456936 Added sl_net_get_interface_info() and sl_wifi_get_interface_info APIs to retrieve detailed stats for AP and Station interfaces in concurrent Wi-Fi mode. Deprecated sl_wifi_get_wireless_info() due to limited support for multi-interface scenarios. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1475983 Added support to configure the open security type option in examples that use HTTP server feature. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1425961 Added a toggle button in the WDT Manager configuration UI to enable or disable the NWP Watchdog Timer (WDT), along with a corresponding value setting for NWP. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1523410 Reduced congestion timeout from 400 ms to 30 ms to improve scan efficiency and performance. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1502519 Handled a negative scenario where the listen interval aligned with the DTIM beacon. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1517229 Fixed a hang in Concurrent Mode where the DUT became unresponsive while attempting to obtain an IPv6 address. None
  • Firmware variants: Standard only
  • OPNs: All except SIWG917M110LGTBA (Lite OPN)
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1532848 Fixed an issue where DUT incorrectly enabled MFP configuration for AP mode with WPA2 security None
  • Firmware variants: Standard only
  • OPNs: All except SIWG917M110LGTBA (Lite OPN)
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1456765 Added support to select TKIP cipher suite for WPA connections to access points supporting mixed encryption modes (TKIP+CCMP). None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1462913 Resolved a stability issue that caused the DUT to hang during continuous DTLS data transfers while operating in WLAN + BLE power save mode on a secure board. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1435744 Support added to handle broadcast de-authentication packets in concurrent station mode. None
  • Firmware variants: Standard only
  • OPNs: All except SIWG917M110LGTBA (Lite OPN)
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1405635 Fixed beacon and broadcast reception issues in congested environments. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1518842 Fixed an issue where the module was incorrectly identifying early beacons from the AP, leading to excessive power consumption during long-run tests. None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART

Chip Enablement#

Added in 4.0.3#

None

Added in 4.0.2#

Added in 4.0.1#

None

Added in 4.0.0#

None

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

New Examples#

Added in 4.0.3#

None

Added in 4.0.2#

None

Added in 4.0.1#

None

Added in 4.0.0#

Example Name Description Supported Software Variants (if applicable) Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

Wi-Fi 6 MIMO Throughput

See README

Demonstrates Wi-Fi 6 2x2 MIMO functionality by connecting to a Wi-Fi 6 access point and running throughput tests. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

WPS Push Button Configuration

See README

Demonstrates using Wi-Fi Protected Setup (WPS) Push Button Configuration (PBC) to connect the device to an access point with minimal user interaction. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Access Point V6

See README

Demonstrates how to set up the device as an IPv6-enabled Wi-Fi Access Point and handle stations joining with IPv6 addresses. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Modified Examples#

Modified in 4.0.3#

None

Modified in 4.0.2#

Example Name Changes Supported Software Variants if applicable Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces
Wireless Test
README
Added support for BRD2708A board for the Wireless Test example. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: BRD2708A (new in 4.0.2 for this example); other supported boards unchanged
SPI, UART
AT Commands
README
Improved AT command handling and BSD socket setup validation (TCP send path and error handling). Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Modified in 4.0.1#

Example Name Changes Supported Software Variants if applicable Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces
Flash Read/Write
README
Updated example to print the data being read and written, improving debug visibility. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART
FW Update Bootloader Xmodem
README
Improved the firmware upgrade flow by ensuring proper deinitialization of the network before reinitialization after an upgrade.
Added error logging for Wi-Fi initialization and deinitialization processes.
Ensured cleanup of the network interface before reinitializing following a firmware upgrade.
Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Modified in 4.0.0#

Example Name Changes Supported Software Variants if applicable Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

AWS Device Shadow

See README

Bug fixes in Wi-Fi connection sequence and error recovery. Improved logging. Minor compatibility improvements. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Powersave Standby Associated

See README

Corrected bugs in standby/resume event sequence. Improved standby re-association reliability. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Powersave Standby Associated TCP Client

See README

Bug fixes for TCP state handling during and after standby. Enhanced error responses and connection recovery. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

TWT TCP Client

See README

Addressed issues in Target Wake Time negotiation. Improved fallback handling. Refined power management routines. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Wi-Fi Throughput

See README

Resolved packet buffer handling bugs. Fixed callback issues for transmit/receive. Improved throughput reporting stability. Increased the optimization level to O3 for the Wi-Fi Throughput example application to improve the performance with ARM Compiler 6 toolchain. Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI

Removed Examples#

Removed in 4.0.3#

None

Removed in 4.0.2#

None

Removed in 4.0.1#

None

Removed in 4.0.0#

None

Deprecated Examples#

Deprecated in 4.0.3#

None

Deprecated in 4.0.2#

None

Deprecated in 4.0.1#

None

Deprecated in 4.0.0#

None

Known Issues and Limitations#

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

Added in 4.0.3#

None

Added in 4.0.2#

None

Added in 4.0.1#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1607773 Extended Scan can incorrectly report AP security as WPA2 when the AP is actually configured as WPA/WPA2 Mixed. None None
  • Software variants: Standard and Lite
  • OPNs: All applicable OPNs
  • Boards: All applicable boards
  • Modes: SOC, NCP
  • Host interfaces: SPI, UART

Added in 4.0.0#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1451898 Added validation for SSID, PSK, and PMK lengths in credential and profile management functions to prevent invalid credentials from being set without error. None None
  • Software variants: Standard and Lite
  • OPNs: All except IC OPNs
  • Boards: All applicable boards
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1494454 APUT sends deauthentication frames with an unspecified reason to a few stations when 8 stations are connected to it in a congested environment. None None
  • Software variants: Standard only
  • OPNs: All except SIWG917M110LGTBA (Lite OPN)
  • Boards: All applicable boards
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1458372 MCS rates drop in between data transfers causing a reduction in SSL RX throughput. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A Command Engine stack overflow can occur if local variables are used in user callback. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
N/A When scanning with low-power mode is enabled, a WLAN sensitivity degradation of 3-6 dB is observed, which might prevent access points at longer ranges from appearing in the scan results. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1199044 Connection issues may be seen with configuring certificate key and programming 4096 bit key and SHA384 / SHA512 certificates in station mode with WPA2 enterprise security. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A Less throughput observed in DL-OFDMA with some access points that enabled low-density parity check coding. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1357685 Extended scan results are not supported with MBSSID feature enabled. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1350997 Advance Scan is not supported in AP mode. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1454142 The beacon reception region is elongated before the PS Poll is sent, leading to increased current consumption, under -85 dB RSSI and 70% congestion. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1439592 SiWx917 power save does not work in station mode when M4 retention is disabled and network processor (NWP) memory is configured at 416 KB or 480 KB. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1443112 CSA with power save enabled may cause the SiWx917 device to re-join the access point. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1218972 When the sl_wifi_enable_target_wake_time API is used, occasional MQTT disconnections may be observed if TWT is configured with longer TWT intervals (>30 seconds) with embedded MQTT + TWT. None Use the sl_wifi_target_wake_time_auto_selection API where these dependencies are internally handled.
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1569122 Repeatedly adding and removing two vendor-specific information elements exceeding 40 bytes in length fails. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1569067 Overriding a vendor-specific IE using a duplicate unique ID in Concurrent Mode causes WLAN connection failure. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1568732 Vendor-specific IEs are unsupported in BGSCAN probe request frames. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1568490 Malformed packets are observed when validating vendor-specific information elements in beacons, probe responses, and association responses. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1557787 Under network congestion, enabling both NAT and PAT features in Concurrent Mode sometimes causes DHCP failures. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: SPI, UART
1569583 IPv6 functionality fails in lwip_mqtt_over_tcp application: Global Address and Gateway Address return invalid IPv6 addresses (::), causing MQTT over TCP to fail with error code -1. Link Local Address is correctly assigned, but Global Address remains invalid. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1569213 AT command at+cal-start fails with error code 4 in at_commands application on SoC with encryption enabled. M4 power save functionality continues to operate correctly despite the command failure. None None
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1517324 Fixed sl_wifi_set_performance_profile() API to prevent data corruption by replacing memcpy between incompatible structures with explicit assignment of listen_interval, monitor_interval, twt_request, and twt_selection fields. Users should migrate to sl_wifi_set_performance_profile_v2() for improved safety and handling. None None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1574418 Using slc generate --toolchain gcc or slc generate --with toolchain_gcc may fail with exclusivity errors due to the wiseconnect_toolchain_gcc_standard component incorrectly providing toolchain_gcc, resulting in a conflict with the SiSDK toolchain_gcc component. If using those two command line options results in exclusivity errors, then you can remove them. Note that in a future WiseConnect release, you might have to reintroduce the toolchain option on the command line. Refer to future WiseConnect release notes for updates on possible behavior changes. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART