Zigbee - 802.15.4 Mesh + BLE Multiprotocol Version 9.0 Revision 3 - Release Notes (Nov 4, 2026)#
This document provides release information for the 802.15.4 Mesh + BLE Multiprotocol SDK.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 9.0#
Concurrent Listening support with CMP on SiMG301x.
Bi-directional Green Power support with CMP Zigbee NCP + OpenThread RCP.
Added in Revision 1#
Per-protocol TX power control in CMP applications.
Added in Revision 2#
None.
Added in Revision 3#
None.
API Changes#
Changed in 9.0#
None.
Changed in Revision 1#
sl_802154_radio_set_scheduler_priorities() removed.
Changed in Revision 2#
None.
Changed in Revision 3#
None.
Bug Fixes#
Targeted quality improvements and bug fixes.
Chip Enablement#
Added in 9.0#
xGM270S Leopard SiP Module GA SW support.
xG301 Explorer Kit and Pro-kit support.
Added in Revision 1#
None.
Added in Revision 2#
None.
Added in Revision 3#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 9.0#
Bi-directional Green Power support with CMP Zigbee NCP + OpenThread RCP
Added bi-directional Green Power support with CMP Zigbee NCP + OT RCP configuration, enabling Green Power Proxy functionality in NCP-RCP multiprotocol applications.
Added in Revision 1#
None.
Added in Revision 2#
None.
Added in Revision 3#
None.
Enhancements#
Added in 9.0#
None.
Added in Revision 1#
In CMP applications, the RAIL MUX now dynamically switches to each protocol's individually configured TX power when that protocol is actively transmitting. Previously, all co-existing 15.4 protocols were constrained to the minimum TX power across all protocol configurations. Additionally, new CLI commands txpower and txpower_set <dBm> are available in CMP applications to independently get and set the OpenThread TX power.
Added in Revision 2#
None.
Added in Revision 3#
None.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
None.
Removed APIs#
Removed in 9.0#
None.
Removed in Revision 1#
Removed API Name | Was Deprecated? |
|---|---|
sl_802154_radio_set_scheduler_priorities | Yes |
Removed in Revision 2#
None.
Removed in Revision 3#
None.
Deprecated APIs#
Deprecated in 9.0#
Deprecated API Name | Planned Removal Date |
|---|---|
2026 Q1 |
Deprecated in Revision 1#
None.
Deprecated in Revision 2#
None.
Deprecated in Revision 3#
None.
Bug Fixes#
Fixed in 9.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1471746 | Fixed an issue where the Zigbee + Bluetooth NCP application examples did not appear in Studio. | N/A | Zigbee + Bluetooth NCP app |
| 1524505 | Fixed an issue that could pass an invalid mac layer packet to cause an assert. | N/A | All OPNs, boards, modes and interfaces |
| 1568095 | Changed default SL_BT_CONTROLLER_BUFFER_MEMORY value for OpenThread NCP + BLE RCP application to work on parts with 96kB RAM. | N/A | OpenThread NCP + BLE RCP app |
Fixed in Revision 1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1569320 | Fixed an issue where CPCd could crash after a BLE scan with an active OT network in the ot-ncp-ftd-ble-rcp application. Updated SL_BTCTRL_RTOS_LINK_LAYER_TASK_STACK_SIZE to 1100 for Series 2 devices. Note: RTOS stack sizes require tuning as needed. | N/A | ot-ncp-ftd-ble-rcp app on Series 2 devices |
| 1569847 | Fixed an issue where gp_transmit_complete_event was not executed in a timely manner due to the Zigbee RTOS task not waking up, causing intermittent bi-directional Green Power commissioning failures. | N/A | CMP Zigbee NCP + OpenThread RCP app with Bi-directional Green Power support |
Fixed in Revision 2#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1625638 | Fixed an issue in the Zigbee + OpenThread FCS CMP application where sl_rail_yield_radio() could yield the radio unexpectedly. |
N/A | Zigbee + OpenThread FCS CMP app |
Fixed in Revision 3#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1591466 | Fixed an issue where BLE GATT characteristic discovery did not return characteristic events when using zigbee_ble_dmp_cli after service discovery. |
N/A | Applications that use zigbee_ble_dmp_cli |
| 1625638 | Fixed an issue in the Zigbee + OpenThread FCS CMP application where Other references: 1642829 |
N/A | Zigbee + OpenThread FCS CMP app |
| 1640172 | Fixed an issue where the Zigbeed application would not compile because of missing header files. | SF case: 00340128 | Zigbeed sample application |
Chip Enablement#
Added in 9.0#
xGM270S Leopard SiP Module: Added GA software support for xGM270S Leopard SiP Module.
xG301 Explorer Kit and Pro-kit Support: Added support for Explorer Kit and Pro-kit boards for xG301 devices.
Added in Revision 1#
None.
Added in Revision 2#
None.
Added in Revision 3#
None.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
New Examples#
Added in 9.0#
| Example Name | Description | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
ot-ncp-ble-rcp See README |
New sample application that integrates DMP BLE-RCP components with OpenThread NCP FTD CPC application, enabling OpenThread NCP with BLE RCP support. | N/A | NCP | All supported OPNs, boards, modes and interfaces | CPC |
|
zigbee_ncp_ot_rcp_uart_gp_multi_rail See README |
New sample application providing bi-directional Green Power support with CMP Zigbee NCP + OT RCP configuration using multi-rail UART interface. | N/A | NCP/RCP | All supported OPNs, boards, modes and interfaces | UART |
Added in Revision 1#
None.
Added in Revision 2#
None.
Added in Revision 3#
None.
Modified Examples#
Modified in 9.0#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Zigbee - BLE Dynamic Multiprotocol Light SED See sample here |
The Zigbee BLE - DynamicMultiprotocolLightSed sample project can now be built for boards with only one LED if the LED1 component is excluded from the project. | N/A | N/A | N/A | N/A |
|
Zigbeed See sample here |
The Zigbeed sample application is now extended with the --conf parameter, so the location of the zigbeed.conf is now configurable and not being hardcoded to /usr/local/etc/zigbeed.conf | N/A | N/A | N/A | N/A |
Modified in Revision 1#
None.
Modified in Revision 2#
None.
Modified in Revision 3#
None.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1209958 | The Zigbee + OpenThread + BLE RCP may stop working in endurance testing (~2 hours) on MG24 and MG21 devices with constant and concurrent traffic on all three stacks. | N/A | None | Zigbee + OpenThread + BLE RCP app |
| 1385052 | Coex-enabled RCP may still occasionally transmit TX ACK after losing the Grant even when Acking is disabled and TX Abort is enabled. | N/A | This will be fixed in future releases. | Coex-enabled RCP |
| 1385486 | TX from coex-enabled RCP may infrequently happen without the request after turning on the non-802.15.4 compliant MAC Holdoff coex option. | N/A | This will be fixed in future releases. | Coex-enabled RCP |
| 1457086 | Coex-enabled EFR32MG24 RCP may sometimes output higher than expected grant denied counts in the PTA counters. | N/A | This will be fixed in future releases. | Coex-enabled RCP |
| 1514786 | Wi-Fi coexistence on SiXG301 is currently not supported. Other references: 1514794, 1515385. |
N/A | This will be supported in future releases. | SiXG301 devices |
| 1569847 | Using the CMP Zigbee NCP + OpenThread RCP application with Bi-directional Green Power support, bi-directional commissioning may intermittently fail. | N/A | None | EFR32xG24 devices |
| 1619497 | The sample app zigbee-ncp-ot-rcp over SPI may fail to form OT network after a Zigbee connection is established. | N/A | None | Series-3 xG301 devices with zigbee-ncp-ot-rcp app over SPI |
| 1625562 | The Zigbeed sample application built for Android 12 may not build correctly when the toolchain_gcc SLC component is selected. |
N/A | None | Zigbeed sample (Android 12 libraries) |