Bluetooth LE SDK Host Stack Version 11.1.1 - Release Notes (Jul 29, 2026)#
The Bluetooth Host Stack is a Bluetooth 6.1-compliant stack that provides the core functionality along with multiple API to simplify development. The core functionality offers both standalone mode, allowing a developer to create and run their application directly on the SoC, or NCP mode, allowing for the use of an external host MCU.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 11.1.1#
None.
Added in 11.1.0#
Periodic advertising ADI and data ID refresh support
Duplicate filtering for periodic advertisement reports
HCI and BGAPI connection handle conversion commands
Connection analyzer maintains synchronization through connection parameter and channel map updates
Configurable RPA randomization intervals for local privacy
RPA refresh notification events for scanner/initiator and advertisers
Read peer resolvable private address from Resolving List
Channel Sounding handover commands and events
API Changes#
Changed in 11.1.1#
None.
Changed in 11.1.0#
New APIs for periodic advertising data management, duplicate filtering, connection handle conversion, connection analyzer LLCP processing, privacy RPA randomization, address refresh events, peer RPA reading, and CS handover
Bug Fixes#
Fixed in 11.1.1#
None.
Fixed in 11.1.0#
Fixed Resolving List local IRK handling when local privacy is not active
Corrected documentation of sl_bt_cs_test_start() antenna_selection parameter
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added in 11.1.1#
None.
Added in 11.1.0#
New flag
SL_BT_PERIODIC_ADVERTISER_INCLUDE_ADVERTISING_DATA_INFORMATIONinsl_bt_periodic_advertiser_flagsenables the inclusion of Advertising Data Information (ADI) in transmitted periodic advertising PDUs.New command
sl_bt_periodic_advertiser_refresh_data_idenables refreshing the Advertising Data ID (DID) without the need to provide the same data again.New mode
sl_bt_sync_report_non_duplicateinsl_bt_sync_reporting_mode_tenables filtering duplicate periodic advertisements.The
bluetooth_feature_linklayer_interfacecomponent provides new commandssl_bt_linklayer_get_hci_connection_handleandsl_bt_linklayer_get_bgapi_connection_handlefor converting between link layer HCI connection handles and the BGAPI host stack connection handles. The application needs to convert between handle types when it uses thelinklayerclass to access low-level link layer functionality that uses connection handles.The
bluetooth_feature_connection_analyzerfeature can now maintain synchronization to the analyzed connection even if connection parameters or channel map is updated. The LLCP events need to be passed from the Central device to the connection analyzer device by the application. Use thebluetooth_feature_connection_analyzer_llcp_reportcomponent and thesl_bt_linklayer_event_info_reporting_enablecommand to enable the LLCP reporting on the Central. Pass the corresponding LLCP events fromsl_bt_evt_linklayer_event_info_reportevents to the connection analyzer device and usesl_bt_connection_analyzer_process_llcp_eventto process the event.New command
sl_bt_gap_set_privacy_mode_with_rpa_randomizationenables configuring local privacy with separate minimum and maximum RPA rotation intervals. When the interval bounds differ, advertiser and central-side RPAs are refreshed at randomized times within the configured range. Keeping the interval bounds equal preserves deterministic rotation behavior.New events
sl_bt_evt_gap_random_address_refreshandsl_bt_evt_advertiser_random_address_refreshnotify the application when the scanner/initiator or a stack-managed advertiser starts using a new private address. The related privacy mode commands document these events.New command
sl_bt_resolving_list_read_peer_resolvable_addressreads the current peer resolvable private address tracked by the controller for a device in the Resolving List.The
bluetooth_feature_cscomponent adds Channel Sounding (CS) handover commands and events to thecsBGAPI class. Use thebluetooth_feature_cs_handover_leaderandbluetooth_feature_cs_handover_followercomponents to enable the corresponding controller-side handover roles. Retrieve CS procedure parameters from the CS Leader, pass them to the CS Follower, and use the handover commands and events to synchronize the Follower to the CS procedure and LE connection and to control scheduled CS procedure execution.
Enhancements#
Added in 11.1.1#
None.
Added in 11.1.0#
None.
Removed Features#
Removed in 11.1.1#
None.
Removed in 11.1.0#
None.
Deprecated Features#
Deprecated in 11.1.1#
None.
Deprecated in 11.1.0#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added in 11.1.1#
None.
Added in 11.1.0#
New API Signature | Deprecated API replaced by this |
|---|---|
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A | |
N/A |
Modified APIs#
Modified in 11.1.1#
None.
Modified in 11.1.0#
None.
Removed APIs#
Removed in 11.1.1#
None.
Removed in 11.1.0#
None.
Deprecated APIs#
Deprecated in 11.1.1#
None.
Deprecated in 11.1.0#
None.
Bug Fixes#
Fixed in 11.1.1#
None.
Fixed in 11.1.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected SW or HW Variants, Modes |
|---|---|---|---|
| 1382779 | Fixed the Resolving List to use an all-zero local IRK when local privacy is not active. Previously, the real local IRK was always used when the local privacy component was present, which caused the controller to drop directed advertising packets addressed to the local device's identity address even when the application had not enabled local privacy. | None | Generic software issue |
| 1529554 | Fixed the GATT server to no longer raise an sl_bt_evt_gatt_server_characteristic_status event with a synthetic "notification and indication enabled" client config for characteristics whose CCCD is user-handled when a connection is opened or re-opened. User-handled CCCDs are owned by the application, so the stack has no client configuration state to report and now skips them in the per-connection client configuration reporting loop. | None | Generic software issue |
| 1586657 | Corrected the documentation of sl_bt_cs_test_start() parameter antenna_selection. The docs now state CS_SYNC usage (including mode-0 packets) and remove the 0xFE loop-mode note for this command. This is a documentation-only fix: runtime behavior is unchanged, and 0xFE was already unsupported for this command. | None | Generic software issue |
Impact of Release Changes#
Impact Statements in 11.1.1#
None.
Impact Statements in 11.1.0#
| Change | Migration Guide | Affected Software Variants if applicable | Affected Modes | Affected OPNs / Boards / OPN Combinations | Affected Host Interfaces |
|---|---|---|---|---|---|
| The Resolving List now sets the local IRK based on whether local privacy is currently active. When local privacy is not active, an all-zero local IRK is used so the controller uses the local device's identity address. Previously, the real local IRK was always used, preventing the local device from receiving directed advertising to its identity address. | Applications that add devices to the Resolving List should be aware that the local IRK is determined at the time the device is added. If the application changes the local privacy mode after adding devices to the Resolving List, it should remove all devices and re-add them to ensure the correct local IRK is used. | All | All | Hardware agnostic | N/A |
Known Issues and Limitations#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1417141 | The OTA DFU fast mode in the Bootloader with Apploader is unreliable due to the chance of packet losses. | None | Use OTA DFU reliable mode. | All |