Bluetooth LE SDK Controller Version 11.1.0 - Release Notes (Jun 23, 2026)#
The Bluetooth SDK is an advanced Bluetooth 6.1-compliant stack that provides all of the core functionality along with multiple API to simplify development. The core functionality offers both standalone mode, allowing a developer to create and run their application directly on the SoC, and NCP mode, allowing for the use of an external host MCU.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added support for Advertising Data Info (ADI) in Periodic Advertising and Periodic Advertising with Responses.
Added Channel Map Update Indication support for the Periodic Advertising advertiser, enabling Adaptive Frequency Hopping with Periodic Advertising in congested RF environments.
Improved Bluetooth LE power efficiency for advertising and peripheral connection use cases.
Extended the Bluetooth LE CTE antenna switching pattern from 50 to 66 antenna IDs.
Moved the selection of active or passive Adaptive Frequency Hopping (AFH) from the Bluetooth Low Energy Controller component to the AFH component.
API Changes#
Added the
SL_BLUETOOTH_COMMON_BUFFER_MEMORY_SIZEconfiguration to the Bluetooth Low Energy Common component.Added
SL_BT_CONTROLLER_RF_RX_PATH_GAIN_DECI_DBandSL_BT_CONTROLLER_RF_TX_PATH_GAIN_DECI_DBconfigurations to the Bluetooth Low Energy Common component.Removed
SL_BT_HOST_ADAPTATION_RADIO_IRQ_PRIORITYandSL_BT_HOST_ADAPTATION_LINKLAYER_IRQ_PRIORITY. UseSL_BT_CONTROLLER_RADIO_IRQ_PRIORITYandSL_BT_CONTROLLER_LINKLAYER_IRQ_PRIORITYin the Bluetooth Low Energy Controller component instead.Deprecated
SL_BT_CONFIG_BUFFER_SIZE,SL_BT_CONFIG_RF_PATH_GAIN_RX, andSL_BT_CONFIG_RF_PATH_GAIN_TXin the Bluetooth Core component, andSL_BT_CONTROLLER_BUFFER_MEMORYin the Bluetooth Low Energy Controller component.
Bug Fixes#
Fixed a Co-Processor Communication (CPC) issue where host reconnection to the BLE endpoint could fail after a client disconnect on multiprotocol applications.
Fixed BLE Extended Advertising TX power handling. The controller now correctly interprets the Host Controller Interface (HCI) "no preference" TX power setting.
Fixed an issue where the scanner could exceed the configured scan window while following extended advertisements, causing higher power consumption.
Fixed an issue where the Bluetooth LE controller did not report support for LE Periodic Advertising in the link layer features.
Connection Analyzer reliability improved: Received Signal Strength Indicator (RSSI) is now reported for every connection event, including cases where the peripheral does not respond.
Corrected the RAIL window scheduler priority configuration naming, with no change to default behavior.
Chip Enablement#
None.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added support for ADI in Periodic Advertising and Periodic Advertising with Responses, improving interoperability with devices expecting this capability.
Added Channel Map Update Indication support for the Periodic Advertising advertiser, enabling Adaptive Frequency Hopping with Periodic Advertising for improved reliability in congested or noisy RF environments.
Enhancements#
Improved Bluetooth LE power efficiency by optimizing Link Layer event handling for advertising and peripheral connection scenarios.
Extended the Bluetooth LE CTE antenna switching pattern length from 50 to 66 antenna IDs, enabling longer AoA/AoD antenna patterns.
Moved the selection of active or passive AFH from the Bluetooth Low Energy Controller component to the AFH component. Documentation was updated to clarify usage and selection.
Removed Features#
Removed the
SL_BT_HOST_ADAPTATION_RADIO_IRQ_PRIORITYandSL_BT_HOST_ADAPTATION_LINKLAYER_IRQ_PRIORITYconfigurations. UseSL_BT_CONTROLLER_RADIO_IRQ_PRIORITYandSL_BT_CONTROLLER_LINKLAYER_IRQ_PRIORITYin the Bluetooth Low Energy Controller component instead.
Deprecated Features#
Deprecated the
SL_BT_CONFIG_BUFFER_SIZE,SL_BT_CONFIG_RF_PATH_GAIN_RX, andSL_BT_CONFIG_RF_PATH_GAIN_TXconfigurations in the Bluetooth Core component, and theSL_BT_CONTROLLER_BUFFER_MEMORYconfiguration in the Bluetooth Low Energy Controller component. Replacement configurations are provided in the Bluetooth Low Energy Common component. Existing projects remain compatible in this release; migration is recommended ahead of removal planned for a future release.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added the
SL_BLUETOOTH_COMMON_BUFFER_MEMORY_SIZEconfiguration to the Bluetooth Low Energy Common component, enabling tuning of the Bluetooth LE Common buffer memory size. Defaults preserve previous behavior.Added the
SL_BT_CONTROLLER_RF_RX_PATH_GAIN_DECI_DBandSL_BT_CONTROLLER_RF_TX_PATH_GAIN_DECI_DBconfigurations to the Bluetooth Low Energy Common component.
Modified APIs#
None.
Removed APIs#
Removed
SL_BT_HOST_ADAPTATION_RADIO_IRQ_PRIORITYandSL_BT_HOST_ADAPTATION_LINKLAYER_IRQ_PRIORITY. UseSL_BT_CONTROLLER_RADIO_IRQ_PRIORITYandSL_BT_CONTROLLER_LINKLAYER_IRQ_PRIORITYfrom the Bluetooth Low Energy Controller component.
Deprecated APIs#
Deprecated
SL_BT_CONFIG_BUFFER_SIZE,SL_BT_CONFIG_RF_PATH_GAIN_RX, andSL_BT_CONFIG_RF_PATH_GAIN_TXin the Bluetooth Core component.Deprecated
SL_BT_CONTROLLER_BUFFER_MEMORYin the Bluetooth Low Energy Controller component.
Bug Fixes#
ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
1647142 | Fixed CPC issue involving host reconnection with remote device. | None | Multiprotocol; CPC |
1635816 | Corrected the RAIL window scheduler priority configuration naming, with no change to default behavior. | None | DMP multiprotocol |
1584863 | Fixed BLE Extended Advertising TX power handling. The controller now correctly interprets the HCI "no preference" TX power setting. | None | All; BLE Extended Advertising |
1580941 | Fixed an issue where the scanner could exceed the configured scan window while following extended advertisements, leading to excessive scan events and higher power consumption. | None | All; BLE Scanner / Extended Advertising |
1556136 | Fixed an issue where the Bluetooth LE controller did not advertise support for LE Periodic Advertising in the link layer features. | None | All; LE Periodic Advertising |
1529614 | Connection Analyzer reliability improved: RSSI is now reported for every connection event, including cases where the peripheral does not respond. | None | All; Connection Analyzer |
Known Issues and Limitations#
ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
1665275 | When configured with the minimum subevent length, Bluetooth Channel Sounding may exceed the 32-subevents per procedure limit and cause processing errors. | None | All; Channel Sounding |
1655386 | Under heavy load when doing mass image updates, ESL tags configured with short sync timeout may briefly lose synchronization and resynchronize, reducing throughput. | None | ESL; PAwR |
1652109 | In Bluetooth Channel Sounding, when only one subevent fits per ACL connection event, the last two subevent results may be reported with the same ACL connection event index. | None | All; Channel Sounding |
1516595 | Angle of departure over connection is not stable on efr32xg24 platforms when using 2Mb PHY. | None | efr32xg24; 2Mb AoD |