Edit

Component Editor#

Click the gear symbol next to an installed configurable component name, or Configure on the component description to open the Component Editor.

proj conf component editor startproj conf component editor start

The Component Editor opens in a new tab. The changes you can make depend on the component.

proj conf component editorproj conf component editor

Changes made here are autosaved in native source format in the associated source files.

proj conf component editor autosaveproj conf component editor autosave

Click View Source to open the configuration header file in an editor in the preferred IDE. If a component has multiple configuration files, the control is View Source Files.

proj conf component editor sourceproj conf component editor source