Troubleshooting#
If any timeout occurs, remove the modules and re-insert them before trying to re-run the application.
Verify if the right commander-cli is present according to the system architecture.
Ensure that the right IP address has been specified while running the commands.
If write is being performed after a previous write is already done, the
--skiploadflag must be added at the end to prevent firmware loading.The flag used to skip device init is
–-skipinit.XOCAL and RADIO commands should be run first after installing the driver or else it will result in a timeout or error.
During the initial write command, the
--skiploadflag must not be used.Ensure that you are using the right bin for the specified purpose. Bin files are usually present in
<path-to-commander>/resources/jlink/Si917/.