Clock API Appendix#
This appendix provides supporting information, definitions, and extended examples for using the Clock Manager application programming interface (API) on the Silicon Labs SiWG917 System-on-Chip (SoC).
It includes a glossary, acronyms, code examples, key references, and frequently asked questions to help you use the Clock Manager API effectively in your applications.
Glossary#
The glossary defines key terms used throughout the Clock Manager API documentation. Use it as a quick reference when you configure clocks on the SiWG917.
M4 core – The primary microcontroller core in the SiWG917, based on the ARM Cortex-M4 architecture. It runs the main application code.
Core clock – The main clock signal driving the CPU or core logic. Also referred to as the processor clock.
Clock tree – The hierarchical structure of all clock sources and how they distribute timing signals to subsystems.
Phase-locked loop (PLL) – A circuit that generates stable, high-frequency clock signals from a lower-frequency reference.
Oscillator – A circuit that produces a periodic signal, typically used as a clock source.
Divider – Hardware logic that reduces a clock frequency by a specific ratio.
Reference clock – The base signal used to derive other clock frequencies.
Blocking delay – A delay mechanism that halts program execution for a defined duration.
Acronyms#
Common acronyms used in this documentation are listed below. Each is defined in full at first mention in the main guide.
Acronym | Definition |
|---|---|
SoC | System-on-Chip |
PLL | Phase-locked loop |
XTAL | Crystal oscillator |
API | Application programming interface |
GSDK | Gecko software development kit |
ULP | Ultra-low power |
Extended Examples#
The following example demonstrates dynamic clock source switching and runtime frequency adjustment using the Clock Manager API.
Use this example as a reference when implementing similar functionality in your application.
// Example: Dynamic clock source switching and frequency adjustment // Initialize the Clock Manager sl_status_t status = sl_si91x_clock_manager_init(); if (status != SL_STATUS_OK) { // Handle initialization error } // Set M4 core clock to use SoC PLL at 120 MHz status = sl_si91x_clock_manager_m4_set_core_clk(M4_SOCPLLCLK, 120000000); if (status != SL_STATUS_OK) { // Handle configuration error } // Change PLL frequency at runtime status = sl_si91x_clock_manager_set_pll_freq(SOC_PLL, 80000000, PLL_REF_CLK_VAL_XTAL); if (status != SL_STATUS_OK) { // Handle PLL error } // Read current core clock source and frequency uint32_t freq = 0; sl_si91x_m4_soc_clk_src_sel_t clk_src = sl_si91x_clock_manager_m4_get_core_clk_src_freq(&freq); // Disable the PLL to save power status = sl_si91x_clock_manager_control_pll(SOC_PLL, false); // Add a 500-ms delay sl_si91x_delay_ms(500);
Tip:
Always verify that the selected clock source is stable before performing source switching or frequency updates.
Next Steps and References#
Refer to the following documentation for more information about the Clock Manager and related subsystems:
Frequently Asked Questions (FAQ)#
Q: What is the purpose of the Clock Manager?
A: The Clock Manager configures and manages clock sources and dividers on the SiWG917, ensuring optimal performance and power efficiency.
Q: Can I change the clock source or frequency at runtime?
A: Yes. The Clock Manager APIs allow dynamic switching and frequency scaling during application execution.
Q: Do I need to reconfigure clocks when changing power states?
A: No. The Clock Manager works with the Power Manager to adjust clock settings automatically during transitions between active and low-power states (such as PS4, PS3, and PS2).
Q: What happens if I select an unstable clock source?
A: The system may behave unpredictably. Always verify clock stability before applying new clock configurations.
Q: How do I add a delay in my application?
A: Use sl_si91x_delay_ms(uint32_t milli_seconds) to insert a blocking delay calibrated to the current core clock.
Q: Where can I find error codes for Clock Manager APIs?
A: See the Status Codes Documentation for all error codes returned by API functions.