sl_wfx_mac_address_t Struct Reference

Structure to handle MAC address format.

Data Fields

uint8_t octet [6]
Table to store a MAC address.

Structure to handle MAC address format.

Definition at line 349 of file sl_wfx_constants.h .

Field Documentation

◆ octet

uint8_t sl_wfx_mac_address_t::octet[6]

Table to store a MAC address.

Definition at line 350 of file sl_wfx_constants.h .

Referenced by sl_wfx_add_blacklist_address() , sl_wfx_add_multicast_address() , sl_wfx_add_whitelist_address() , sl_wfx_disconnect_ap_client_command() , sl_wfx_get_ap_client_signal_strength() , sl_wfx_remove_multicast_address() , and sl_wfx_set_mac_address() .


The documentation for this struct was generated from the following file:
  • sl_wfx_constants.h