ENUM
Enumerations |
|
enum | sl_wfx_register_address_t |
Enum listing the registers of the WFx solution.
|
|
enum | sl_wfx_state_t |
Enum listing the different state of the WFx chip.
|
|
enum |
sl_wfx_interface_t
{
SL_WFX_STA_INTERFACE = 0x00, SL_WFX_SOFTAP_INTERFACE = 0x01 } |
Enum listing available interfaces in WFx Wi-Fi solution.
|
|
enum |
sl_wfx_antenna_config_t
{
SL_WFX_ANTENNA_1_ONLY = 0, SL_WFX_ANTENNA_2_ONLY , SL_WFX_ANTENNA_TX1_RX2 , SL_WFX_ANTENNA_TX2_RX1 , SL_WFX_ANTENNA_DIVERSITY } |
Enum listing the different antenna configurations.
|
|
enum |
sl_wfx_received_message_type_t
{
SL_WFX_CONFIRMATION_MESSAGE = 0, SL_WFX_INDICATION_MESSAGE = 1, SL_WFX_MANAGEMENT_MESSAGE = 2, SL_WFX_ETHERNET_DATA_MESSAGE = 3 } |
Enum listing different message types received from WFx.
|
|
enum | sl_wfx_buffer_type_t |
Enumerates the different types of buffer.
|
|
enum | sl_wfx_host_bus_transfer_type_t |
Enumerates the different types of bus transfers.
|
|
enum | sl_wfx_secure_link_mode_t |
Enum listing the different secure link mode of a part.
|
|
enum | sl_wfx_securelink_renegotiation_state_t |
Enumerates the states of the secure link key renegotiation.
|
Enumeration Type Documentation
◆ sl_wfx_antenna_config_t
Enum listing the different antenna configurations.
Definition at line
286
of file
sl_wfx_constants.h
.
◆ sl_wfx_interface_t
enum sl_wfx_interface_t |
Enum listing available interfaces in WFx Wi-Fi solution.
For convenience, interface 0 is associated with the station interface and interface 1 is associated with the softap interface.
Enumerator | |
---|---|
SL_WFX_STA_INTERFACE |
Interface 0, linked to the station. |
SL_WFX_SOFTAP_INTERFACE |
Interface 1, linked to the softap. |
Definition at line
277
of file
sl_wfx_constants.h
.
◆ sl_wfx_received_message_type_t
Enum listing different message types received from WFx.
The information is found in the control register using SL_WFX_CONT_FRAME_TYPE_INFO mask.
Definition at line
300
of file
sl_wfx_constants.h
.