ERROR_IDSGENERAL_API

Enumerations

enum sl_wfx_error_t {
SL_WFX_ERROR_FIRMWARE_ROLLBACK = 0x0,
SL_WFX_ERROR_DEPRECATED_0 = 0x1,
SL_WFX_ERROR_DEPRECATED_1 = 0x2,
SL_WFX_ERROR_INVALID_SESSION_KEY = 0x3,
SL_WFX_ERROR_OOR_VOLTAGE = 0x4,
SL_WFX_ERROR_PDS_VERSION = 0x5,
SL_WFX_ERROR_OOR_TEMPERATURE = 0x6,
SL_WFX_ERROR_REQ_DURING_KEY_EXCHANGE = 0x7,
SL_WFX_ERROR_DEPRECATED_2 = 0x8,
SL_WFX_ERROR_DEPRECATED_3 = 0x9,
SL_WFX_ERROR_SECURELINK_DECRYPTION = 0xa,
SL_WFX_ERROR_SECURELINK_WRONG_ENCRYPTION_STATE = 0xb,
SL_WFX_SPI_OR_SDIO_FREQ_TOO_LOW = 0xc,
SL_WFX_ERROR_DEPRECATED_4 = 0xd,
SL_WFX_ERROR_DEPRECATED_5 = 0xe,
SL_WFX_HIF_BUS_ERROR = 0xf,
SL_WFX_PDS_TESTFEATURE_MODE_ERROR = 0x10,
SL_WFX_ERROR_SECURELINK_EXPECTED_BITMAP = 0x11
}
specifies the type of error reported by the indication message sl_wfx_error_ind_body_t

Enumeration Type Documentation

◆ sl_wfx_error_t

specifies the type of error reported by the indication message sl_wfx_error_ind_body_t

Enumerator
SL_WFX_ERROR_FIRMWARE_ROLLBACK

Firmware rollback error, no data returned.

SL_WFX_ERROR_DEPRECATED_0

Not used anymore.

SL_WFX_ERROR_DEPRECATED_1

Not used anymore.

SL_WFX_ERROR_INVALID_SESSION_KEY

Secure Link Session key is invalid (probably not initialized)

SL_WFX_ERROR_OOR_VOLTAGE

Out-of-range power supply voltage detected, the last voltage value is returned. Param: measured voltage (mV)

SL_WFX_ERROR_PDS_VERSION

Wrong PDS version detected, no data returned.

SL_WFX_ERROR_OOR_TEMPERATURE

Out-of-range temperature, no data returned.

SL_WFX_ERROR_REQ_DURING_KEY_EXCHANGE

Requests from Host are forbidden until the end of key exchange (Host should wait for the associated indication)

SL_WFX_ERROR_DEPRECATED_2

Not used anymore.

SL_WFX_ERROR_DEPRECATED_3

Not used anymore.

SL_WFX_ERROR_SECURELINK_DECRYPTION

An error occured during message decryption (can be a counter mismatch or wrong CCM tag)

SL_WFX_ERROR_SECURELINK_WRONG_ENCRYPTION_STATE

Encryption state of the received message doesn't match the SecureLink bitmap. Param: was encrypted.

SL_WFX_SPI_OR_SDIO_FREQ_TOO_LOW

SPI or SDIO bus clock is too slow (<1kHz)

SL_WFX_ERROR_DEPRECATED_4

Not used anymore.

SL_WFX_ERROR_DEPRECATED_5

Not used anymore.

SL_WFX_HIF_BUS_ERROR

HIF HW has reported an error. Param: HIF status register.

SL_WFX_PDS_TESTFEATURE_MODE_ERROR

Unknown TestFeatureMode during test feature init.

SL_WFX_ERROR_SECURELINK_EXPECTED_BITMAP

The SecureLink bitmap must be configured right after key exchange.

Definition at line 27 of file sl_wfx_general_error_api.h .