Configuring Common BLE Parameters#
The following sections describe common BLE configuration parameters that enable/disable or configure various BLE features of the SiWx917 Open Source Driver (OSD).
Note: The following
insmodcommand may be used to configure multiple parameters at the same time. Note that this only applies to the parameters below that are configuring usinginsmod.Replace
module_paramwith the module parameter to be configured and <value> with the corresponding value that needs to be assigned. Module parameters in this section are grouped according to the corresponding feature.insmod rsi_91x.ko [module_param = <value>], [module_param = <value>], ... , [module_param = <value>]
insmod rsi_91x.ko bt_rf_type = < value >: This variable selects the BT RF TYPE which the module has to operate. The following are the possible values:
0 - EXTERNAL RF
1 - INTERNAL RF (Default)
For example, bt_rf_type = 1 sets bt rf type to Internal RF.
insmod rsi_91x.ko ble_tx_pwr_inx = < value > :This module param selects the BLE_TX_PWR index value. Default Value for BLE Tx Power Index is 30. The following are the possible values:
For the BLE Tx LP Chain: 1 - 63 (0, 32 are invalid)
For the BLE Tx HP Chain: 64 - 76
For example, you can set the value as shown here.
BLE_TX_PWR_INX=0x1einsmod rsi_91x.ko ble_power_save_options = < value >: This variable selects the BLE_PWR_SAVE_OPTIONS mode value. The following are the possible values.
BIT(0) - BLE_DUTY_CYCLING
BIT(1) - BLR_DUTY_CYCLING
BIT(2) - BLE_PWR_SAVE_4X_MODE
Default value is 2 i.e. BIT(1)- BLR_DUTY_CYCLING is set.
insmod rsi_91x.ko ble_roles = < value >: This varialble sets the number of BLE roles allowed.
BIT[3:0] represents the number of central roles allowed.
BIT[7:4] represents the number of peripheral roles allowed.
Default value is set to 19.
insmod rsi_91x.ko bt_bdr_mode = < value >: BDR mode in classic.
BIT(0) - BDR only selection
BIT(1) - BDR in LP chain selection
Default value is bt_bdr_mode = 0.
insmod rsi_91x.ko bt_rf_tx_power_mode = < value >:
Default value is 0.
insmod rsi_91x.ko bt_rf_rx_power_mode = < value >:
Default value is 0.
insmod rsi_91x.ko bt_feature_bitmap = < value >: The bt_feature map can be assigned a value as explained below.
BIT[0] - For Enabling role switch from host set this bit to 1
BIT[1] - For Enabling sniff from host set this bit to 1
BIT[5] - For Enabling BT Spoof MAC address i.e to use HARDCODE_MAC_ADDR in BT this bit should be set to 1
BIT[7:3] - Reserved
Default value is 0.