BLE Power Save Mode#
Vendor-specific HCI commands configure the device in power save mode. The module supports Low Power (LP) and Ultra-Low Power (ULP) modes. These are explained in more detail in the Power Save Modes and Configuration section of Wi-Fi Powersave mode. The LP and ULP modes are supported with the SDIO interface.
Run the following command to enable the BLE power save.
hcitool -i <hciX> cmd 0x3F 0x0003 <sleep enable/disable> <sleep mode> <sleep duration>< hciX > - hci interface
< sleep enable/disable > - 0x01 -sleep enable, 0x00 - sleep disable
< Sleep mode > - 0x02 – ULP (Ultra Low Power) mode
< Sleep Duration> - used for sleep duration in Standby mode (in milliseconds) and Range is 0x00 – 0xFF
Example:
hcitool -i hci0 cmd 0x3f 0x0003 0x01 0x02 0xffNote: In Wi-Fi + BLE coexistence mode, give both BLE and Wi-Fi power save commands to enable power save. See the Power Save Modes and Configuration section for Wi-Fi Powersave mode related information.