Capturing Network Traffic#
This section provides comprehensive guides for capturing network traffic from Silicon Labs hardware using Wireshark integrated with Simplicity Device Manager (SDM).
Available Capture Methods#
Choose the method that best fits your workflow:
UI-Based Capturing#
Use the SDM graphical interface to:
Visually manage adapters and capture interfaces.
Configure adapters using drag-and-drop actions.
Easily set up single or multi-adapter captures.
CLI-Based Capturing#
Use SDM command-line tools to:
Scripted and automated workflows
Programmatic capture interface management
Integration with development pipelines
What You Can Capture#
Both methods support capturing traffic from:
Single adapters - Monitor traffic from one specific device.
Multiple adapters - Aggregate traffic from multiple devices into a single capture stream.
Supported protocols - Wi-SUN, Zigbee, and Thread.
Before You Start#
Complete the Getting Started setup guide to ensure Wireshark is properly configured with SDM.
Need Help?#
See the FAQ section for troubleshooting common issues and advanced configuration options.