Application Components#
WiSeConnectâ„¢ SDK v3.x has revamped the component organization such that almost none of the v2.x components remain in v3.x.
The following sections provide a list of v3.x components.
The component category path is listed for each component, specifying how to navigate to the component in Simplicity Studio. Components are listed in alphabetical order of the component category path.
BLE#
Component Name | Component Category Path |
|---|---|
ble | Unknown |
Wi-Fi#
Component Name | Component Category Path |
|---|---|
Wi-Fi resources | Resources |
Si91x Support Library | Wi-Fi |
Wi-Fi Core | Wi-Fi |
Network Management#
Component Name | Component Category Path |
|---|---|
Network Manager | Networking > Core |
SL TLS | Networking > Core |
Basic Data Manager | Networking > Data Management |
NVM3 Data Manager | Networking > Data Management |
BSD Sockets | Networking > Sockets |
Si91x Driver#
Component Name | Component Category Path |
|---|---|
Network Offload | Devices > Si91x |
Basic buffers | Devices > Si91x > Memory |
Hosted LwIP Network Stack | Devices > Si91x > Networking |
Si91x SoC | Devices > Si91x > Si91x Driver |
si91x_core | Unknown |
Si91x Platform#
Component Name | Component Category Path |
|---|---|
BRD4325A | Platform > Board > Radio Board |
BRD4325B | Platform > Board > Radio Board |
BRD4325C | Platform > Board > Radio Board |
BRD4325G | Platform > Board > Radio Board |
Memory LCD with 917's SPI driver | Platform > si91x > core |
SL CALENDAR | Platform > Board > si91x > Drivers |
SL CONFIG TIMER | Platform > Board > si91x > Drivers |
SL DMA | Platform > Board > si91x > Drivers |
SL GPIO | Platform > Board > si91x > Drivers |
SL GSPI | Platform > Board > si91x > Drivers |
SL I2C | Platform > Board > si91x > Drivers |
SL IOSTREAM USART | Platform > Board > si91x > Drivers |
SL SIO | Platform > Board > si91x > Drivers |
SL SSI | Platform > Board > si91x > Drivers |
SL ULP | Platform > Board > si91x > Drivers |
SL USART | Platform > Board > si91x > Drivers |
SL WDT | Platform > Board > si91x > Drivers |
si917_memory_default_config | Platform > Board > si91x > core |
Toolchain for ARM | Platform > Board > si91x > Toolchain |
ULP Timer Instance | Platform > Board > si91x > Drivers |
Protocols and Services#
Component Name | Component Category Path |
|---|---|
aws_sdk | Unknown |
http_client | Unknown |
mqtt | Unknown |
sntp | Unknown |