Asynchronous API Invocation#
WiSeConnectâ„¢ SDK v3.x has common API functions for both synchronous and asynchronous processing, while v2.x has different functions for synchronous and asynchronous processing.
For example, in v3.x, the sl_wifi_connect() function is invoked with a timeout_ms parameter value of 0 to connect to a Wi-Fi access point (AP) asynchronously, and a value other than 0 to connect synchronously. In v2.x, the rsi_wlan_connect_async() function is invoked to connect to a Wi-Fi AP asynchronously, and rsi_wlan_connect() to connect synchronously.