Functionality Breaks between SDK v2.x and v3.x#
The following are the features in WiSeConnect™ SDK v2.x that are not supported in v3.x:
Asynchronous sockets - since they are incompatible with the API standards for BSD and IoT sockets.
Synchronous scanning of Wi-Fi Service Set Identifiers (SSIDs) - the SDK supports asynchronous scanning.
Bare Metal applications - applications must run on the Real-Time Operating System (RTOS).
File Transfer Protocol (FTP)
Compiling applications with STM35™ and RT595™ processors as external hosts.