Calendar#
Modules#
Typedefs#
Renaming clock type enum.
Renaming datetime structure.
Renaming month structure.
Renaming days of week structure.
Typedef for the function pointer of the callback function.
Functions#
Enumeration to represent time conversion format.
Enumeration to represent different rc clock calibration configurations.
Enumeration to represent different ro clock calibration configurations.
Configuration and initialization of Calendar i.e., RTC clock.
Set the date and time of the Calendar RTC.
Get the date and time of an existing Calendar RTC.
Calibrate the RC Clock.
Calibrate the RO Clock.
Register the callback of the msec trigger and enable it.
Register the callback of the sec trigger and enable it.
Register the callback of the alarm trigger and enable it.
Unregister the callback of the msec trigger and disable it.
Unregister the callback of the sec trigger and disable it.
Unregister the callback of the alarm trigger and disable it.
Set the date and time of new alarm in RTC.
Get the date and time of an existing alarm in RTC.
Build the structure for date-time configuration.
Convert Unix timestamp to NTP timestamp.
Convert NTP timestamp to Unix timestamp.
Return the state of msec trigger of RTC (enabled or disabled).
Return the state of sec trigger of RTC (enabled or disabled).
Return the state of alarm trigger of RTC (enabled or disabled).
Start the Calendar RTC.
Stop the Calendar RTC.
Initialize the calibration for Calendar clocks.
Clear the msec trigger.
Clear the sec trigger.
Clear the alarm trigger.
De-initialize calendar operation.
De-initialize calendar operation.
Get the calendar version.
Macros#
Alarm IRQ Handler.
RTC IRQ Handler.
Alarm NVIQ enable.
RTC NVIQ enable.
Time Conversion format enum declaration.
Time Conversion format enum declaration.
Time Conversion format enum declaration.
Typedef Documentation#
sl_calendar_datetime_config_t#
typedef RTC_TIME_CONFIG_T sl_calendar_datetime_config_t
Renaming datetime structure.
sl_calendar_days_of_week_t#
typedef RTC_DAY_OF_WEEK_T sl_calendar_days_of_week_t
Renaming days of week structure.
calendar_callback_t#
typedef void(* calendar_callback_t) (void) )(void)
Typedef for the function pointer of the callback function.
Function Documentation#
TIME_CONVERSION_ENUM#
TIME_CONVERSION_ENUM (time_conversion_enum )
Enumeration to represent time conversion format.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| time_conversion_enum | N/A |
RC_CLOCK_CALIBRATION_ENUM#
RC_CLOCK_CALIBRATION_ENUM (rc_clock_calibration_enum )
Enumeration to represent different rc clock calibration configurations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| rc_clock_calibration_enum | N/A |
RO_CLOCK_CALIBRATION_ENUM#
RO_CLOCK_CALIBRATION_ENUM (ro_clock_calibration_enum )
Enumeration to represent different ro clock calibration configurations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ro_clock_calibration_enum | N/A |
sl_si91x_calendar_set_configuration#
sl_status_t sl_si91x_calendar_set_configuration (sl_calendar_clock_t clock_type)
Configuration and initialization of Calendar i.e., RTC clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_clock_t | [in] | clock_type | (sl_calendar_clock_t) Enum for RTC Clock Type (RO, RC or XTAL) |
Returns
status 0 if successful, else errorcode. SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success SL_STATUS_FAIL (0x0001) - The function is failed
sl_si91x_calendar_set_date_time#
sl_status_t sl_si91x_calendar_set_date_time (sl_calendar_datetime_config_t * config)
Set the date and time of the Calendar RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | config | (sl_calendar_datetime_config_t) Pointer to the Date Configuration Structure |
Returns
status 0 if successful, else error code SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success
sl_si91x_calendar_get_date_time#
sl_status_t sl_si91x_calendar_get_date_time (sl_calendar_datetime_config_t * config)
Get the date and time of an existing Calendar RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | config | (sl_calendar_datetime_config_t) Pointer to the Date Configuration Structure |
Returns
status 0 if successful, else error code SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success
sl_si91x_calendar_rcclk_calibration#
sl_status_t sl_si91x_calendar_rcclk_calibration (clock_calibration_config_t * clock_calibration_config)
Calibrate the RC Clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| clock_calibration_config_t * | [in] | clock_calibration_config | (clock_calibration_config_t) pointer to the clock calibration structure |
Returns
status 0 if successful, else error code SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success
sl_si91x_calendar_roclk_calibration#
sl_status_t sl_si91x_calendar_roclk_calibration (clock_calibration_config_t * clock_calibration_config)
Calibrate the RO Clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| clock_calibration_config_t * | [in] | clock_calibration_config | (clock_calibration_config_t) pointer to the clock calibration structure |
Returns
status 0 if successful, else error code SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success
sl_si91x_calendar_register_msec_trigger_callback#
sl_status_t sl_si91x_calendar_register_msec_trigger_callback (calendar_callback_t callback)
Register the callback of the msec trigger and enable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| calendar_callback_t | [in] | callback | (function pointer) Callback function pointer to be called when msec interrupt is triggered |
Returns
status 0 if successful, else error code SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_OK (0x0000) - Success SL_STATUS_BUSY (0x0004) - The callback is already registered, unregister previous callback before registering new one
sl_si91x_calendar_register_sec_trigger_callback#
sl_status_t sl_si91x_calendar_register_sec_trigger_callback (calendar_callback_t callback)
Register the callback of the sec trigger and enable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| calendar_callback_t | [in] | callback | (function pointer) Callback function pointer to be called when sec interrupt is triggered |
Returns
status 0 if successful, else error code SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_OK (0x0000) - Success SL_STATUS_BUSY (0x0004) - The callback is already registered, unregister previous callback before registering new one
sl_si91x_calendar_register_alarm_trigger_callback#
sl_status_t sl_si91x_calendar_register_alarm_trigger_callback (calendar_callback_t callback)
Register the callback of the alarm trigger and enable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| calendar_callback_t | [in] | callback | (function pointer) Callback function pointer to be called when alarm interrupt is triggered |
Returns
status 0 if successful, else error code SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_OK (0x0000) - Success SL_STATUS_BUSY (0x0004) - The callback is already registered, unregister previous callback before registering new one
sl_si91x_calendar_unregister_msec_trigger_callback#
sl_status_t sl_si91x_calendar_unregister_msec_trigger_callback (void )
Unregister the callback of the msec trigger and disable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_FAIL (0x0001) - The function is failed
sl_si91x_calendar_unregister_sec_trigger_callback#
sl_status_t sl_si91x_calendar_unregister_sec_trigger_callback (void )
Unregister the callback of the sec trigger and disable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_FAIL (0x0001) - The function is failed
sl_si91x_calendar_unregister_alarm_trigger_callback#
sl_status_t sl_si91x_calendar_unregister_alarm_trigger_callback (void )
Unregister the callback of the alarm trigger and disable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_si91x_calendar_register_alarm_trigger_callback
Returns
status 0 if successful, else error code SL_STATUS_OK (0x0000) - Success SL_STATUS_FAIL (0x0001) - The function is failed
sl_si91x_calendar_set_alarm#
sl_status_t sl_si91x_calendar_set_alarm (sl_calendar_datetime_config_t * alarm)
Set the date and time of new alarm in RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | alarm | Pointer to the Date Configuration Structure |
Returns
status 0 if successful, else error code SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success
sl_si91x_calendar_get_alarm#
sl_status_t sl_si91x_calendar_get_alarm (sl_calendar_datetime_config_t * alarm)
Get the date and time of an existing alarm in RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | alarm | Pointer to the Date Configuration Structure |
Returns
status 0 if successful, else error code SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success
sl_si91x_calendar_build_datetime_struct#
sl_status_t sl_si91x_calendar_build_datetime_struct (sl_calendar_datetime_config_t * date, uint8_t Century, uint8_t Year, sl_calendar_month_t Month, sl_calendar_days_of_week_t DayOfWeek, uint8_t Day, uint8_t Hour, uint8_t Minute, uint8_t Second, uint16_t Milliseconds)
Build the structure for date-time configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | date | Pointer to the Date Configuration Structure |
| uint8_t | [in] | Century | (uint8_t) Century (0-4) |
| uint8_t | [in] | Year | (uint8_t) Year (1-99) + (Century * 1000) |
| sl_calendar_month_t | [in] | Month | (enum) Month from the RTC_MONTH_T enum |
| sl_calendar_days_of_week_t | [in] | DayOfWeek | (enum) Day of Week from the RTC_DAY_OF_WEEK_T enum |
| uint8_t | [in] | Day | Day (uint8_t) (1-31) |
| uint8_t | [in] | Hour | Hour (uint8_t) (0-23) |
| uint8_t | [in] | Minute | Minutes (uint8_t) (0-59) |
| uint8_t | [in] | Second | Seconds (uint8_t) (0-59) |
| uint16_t | [in] | Milliseconds | Milliseconds (uint16_t) (0-999) |
Returns
status 0 if successful, else error code SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success
sl_si91x_calendar_convert_unix_time_to_ntp_time#
sl_status_t sl_si91x_calendar_convert_unix_time_to_ntp_time (uint32_t time, uint32_t * ntp_time)
Convert Unix timestamp to NTP timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | time | (uint32_t) Unix timestamp |
| uint32_t * | [in] | ntp_time | (uint32_t) variable to store NTP timestamp |
Returns
status 0 if successful, else error code SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success
sl_si91x_calendar_convert_ntp_time_to_unix_time#
sl_status_t sl_si91x_calendar_convert_ntp_time_to_unix_time (uint32_t ntp_time, uint32_t * time)
Convert NTP timestamp to Unix timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | ntp_time | (uint32_t) NTP timestamp |
| uint32_t * | [in] | time | (uint32_t) variable to store Unix timestamp |
Returns
status 0 if successful, else error code SL_STATUS_NULL_POINTER (0x0022) - The parameter is null pointer SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid SL_STATUS_OK (0x0000) - Success
sl_si91x_calendar_is_msec_trigger_enabled#
boolean_t sl_si91x_calendar_is_msec_trigger_enabled (void )
Return the state of msec trigger of RTC (enabled or disabled).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
(boolean)true if trigger is enabled, false otherwise
sl_si91x_calendar_is_sec_trigger_enabled#
boolean_t sl_si91x_calendar_is_sec_trigger_enabled (void )
Return the state of sec trigger of RTC (enabled or disabled).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
(boolean)true if trigger is enabled, false otherwise
sl_si91x_calendar_is_alarm_trigger_enabled#
boolean_t sl_si91x_calendar_is_alarm_trigger_enabled (void )
Return the state of alarm trigger of RTC (enabled or disabled).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_si91x_calendar_register_alarm_trigger_callback
Returns
(boolean)true if trigger is enabled, false otherwise
sl_si91x_calendar_rtc_start#
__STATIC_INLINE void sl_si91x_calendar_rtc_start (void )
Start the Calendar RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_calendar_rtc_stop#
__STATIC_INLINE void sl_si91x_calendar_rtc_stop (void )
Stop the Calendar RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_calendar_calibration_init#
__STATIC_INLINE void sl_si91x_calendar_calibration_init (void )
Initialize the calibration for Calendar clocks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_calendar_clear_msec_trigger#
__STATIC_INLINE void sl_si91x_calendar_clear_msec_trigger (void )
Clear the msec trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_calendar_clear_sec_trigger#
__STATIC_INLINE void sl_si91x_calendar_clear_sec_trigger (void )
Clear the sec trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_calendar_clear_alarm_trigger#
__STATIC_INLINE void sl_si91x_calendar_clear_alarm_trigger (void )
Clear the alarm trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_calendar_init#
__STATIC_INLINE void sl_si91x_calendar_init (void )
De-initialize calendar operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_calendar_deinit#
__STATIC_INLINE void sl_si91x_calendar_deinit (void )
De-initialize calendar operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
none
sl_si91x_calendar_get_version#
sl_calendar_version_t sl_si91x_calendar_get_version (void )
Get the calendar version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | [in] |
This function is used to know the calendar version.
Returns
sl_calendar_version_t type version