Direct Memory Access#

Modules#

sl_dma_callback_t

sl_dma_init_t

sl_channel_data_t

sl_dma_xfer_t

Enumerations#

enum
SL_DMA_MEMORY_TO_MEMORY
SL_DMA_MEMORY_TO_PERIPHERAL
SL_PERIPHERAL_TO_MEMORY
}

Enumeration holds transfer types of DMA.

enum
SL_DMA_BASIC_MODE = UDMA_MODE_BASIC
SL_DMA_PINGPONG_MODE = UDMA_MODE_PINGPONG
}

Enumeration holds transfer modes of DMA.

enum
SL_USART0_ACK = 0x01
SL_UART1_ACK = 0x02
SL_UART3_ACK = 0x03
SL_SSI_SLAVE_ACK = 0x04
SL_SSI_MASTER_ACK = 0x05
SL_SSI1_SLAVE_ACK = 0x06
SL_I2C_ACK = 0x07
}

Enumeration holds peripheral ACK signals to DMA.

enum
SL_TRANSFER_SIZE_32 = SRC_SIZE_32
SL_TRANSFER_SIZE_16 = SRC_SIZE_16
SL_TRANSFER_SIZE_8 = SRC_SIZE_8
}

Enumeration holds DMA transfer sizes.

enum
SL_TRANSFER_SRC_INC_32 = SRC_INC_32
SL_TRANSFER_SRC_INC_16 = SRC_INC_16
SL_TRANSFER_SRC_INC_8 = SRC_INC_8
SL_TRANSFER_SRC_INC_NONE = SRC_INC_NONE
SL_TRANSFER_DST_INC_32 = DST_INC_32
SL_TRANSFER_DST_INC_16 = DST_INC_16
SL_TRANSFER_DST_INC_8 = DST_INC_8
SL_TRANSFER_DST_INC_NONE = DST_INC_NONE
}

Enumeration holds DMA transfer address increment for source and destination.

enum
SL_DMA_TRANSFER_DONE_CB = 1
SL_DMA_ERROR_CB = 2
}

Enumeration holds 8-bit codes which are used by callback_type in sl_si91x_dma_unregister_callbacks function.

Typedefs#

typedef void(*
sl_dma_transfer_complete)(uint32_t channel, void *data)

Typedef for user supplied callback function which is called when a DMA transfer completes.

typedef void(*
sl_dma_error)(uint32_t channel, void *data)

Typedef for user supplied callback function which is called when a DMA error occurs.

Variables#

DMA driver channel allocator.

Functions#

sl_status_t
sl_si91x_dma_init(sl_dma_init_t *dma_init)

Initialize DMA peripheral by enabling DMA clock and clearing DMA interrupts.

sl_status_t
sl_si91x_dma_deinit(uint32_t dma_number)

Deinitialize the DMA module by disabling peripheral clock and interrupts, if there is no ongoing DMA transfer.

sl_status_t
sl_si91x_dma_allocate_channel(uint32_t dma_number, uint32_t *channel_no, uint32_t priority)

Check the available DMA channel and allocate the channel.

sl_status_t
sl_si91x_dma_deallocate_channel(uint32_t dma_number, uint32_t channel_no)

Deallocate the DMA channel if there is no ongoing transfer on channel.

sl_status_t
sl_si91x_dma_register_callbacks(uint32_t dma_number, uint32_t channel_no, sl_dma_callback_t *callback_t)

Register DMA callbacks (transfer complete & error).

sl_status_t
sl_si91x_dma_unregister_callbacks(uint32_t dma_number, uint32_t channel_no, uint8_t callback_type)

Unregister DMA callbacks (transfer complete & error).

sl_status_t
sl_si91x_dma_transfer(uint32_t dma_number, uint32_t channel_no, sl_dma_xfer_t *dma_transfer_t)

Configure the DMA channel descriptor and initiate DMA transfer.

sl_status_t
sl_si91x_dma_simple_transfer(uint32_t dma_number, uint32_t channel_no, void *src_addr, void *dst_addr, uint32_t data_size)

Configure the DMA channel descriptor and initiate simple memory to memory DMA transfer.

sl_status_t
sl_si91x_dma_stop_transfer(uint32_t dma_number, uint32_t channel_no)

Stop any active transfer on a channel.

sl_status_t
sl_si91x_dma_channel_status_get(uint32_t dma_number, uint32_t channel_no)

Return the channel status i.e., whether the channel is allocated/busy/idle.

Macros#

#define
SL_STATUS_DMA_CHANNEL_ALLOCATED (sl_status_t)0x45
#define
SL_STATUS_DMA_NO_CHANNEL_AVAILABLE (sl_status_t)0x46
#define
SL_STATUS_DMA_CHANNEL_ALREADY_UNALLOCATED (sl_status_t)0X47
#define
SL_STATUS_DMA_CHANNEL_UNALLOCATED (sl_status_t)0X48
#define
SL_CHANNEL_COUNT 32
#define
ALTERNATE_DESCRIPTOR_DISABLE 0
#define
ALTERNATE_DESCRIPTOR_ENABLE 1
#define
BURST_REQUEST_ENABLE 1
#define
BURST_REQUEST_DISABLE 0
#define
CHANNEL_PRIO_DISABLE 0
#define
CHANNEL_PRIO_ENABLE 1
#define
PERIPHERAL_ACK_DISABLE 0
#define
PERIPHERAL_REQUEST_DISABLE 0
#define
PERIPHERAL_REQUEST_ENABLE 1
#define
REQUEST_MASK_DISABLE 0
#define
NEXT_BURST_ENABLE 1
#define
NEXT_BURST_DISABLE 0
#define
SOURCE_PROTECT_CONTROL_DISABLE 0x000
#define
DESTINATION_PROTECT_CONTROL_DISABLE 0x000

Enumeration Documentation#

sl_dma_transfer_type_t#

sl_dma_transfer_type_t

Enumeration holds transfer types of DMA.

Enumerator
SL_DMA_MEMORY_TO_MEMORY

Memory to memory transfer.

SL_DMA_MEMORY_TO_PERIPHERAL

Memory to peripheral transfer.

SL_PERIPHERAL_TO_MEMORY

Peripheral to memory transfer.


sl_dma_transfer_mode_t#

sl_dma_transfer_mode_t

Enumeration holds transfer modes of DMA.

Enumerator
SL_DMA_BASIC_MODE

Basic DMA mode.

SL_DMA_PINGPONG_MODE

Ping pong mode.


sl_dma_peripheral_ack_t#

sl_dma_peripheral_ack_t

Enumeration holds peripheral ACK signals to DMA.

Enumerator
SL_USART0_ACK

ACK code for USART0.

SL_UART1_ACK

ACK code for UART1.

SL_UART3_ACK

ACK code for UART3.

SL_SSI_SLAVE_ACK

ACK code for SSI slave.

SL_SSI_MASTER_ACK

ACK code for SSI master.

SL_SSI1_SLAVE_ACK

ACK code for SSI1.

SL_I2C_ACK

ACK code for I2C.


sl_dma_transfer_size_t#

sl_dma_transfer_size_t

Enumeration holds DMA transfer sizes.

Enumerator
SL_TRANSFER_SIZE_32

4 bytes transfer size

SL_TRANSFER_SIZE_16

2 bytes transfer size

SL_TRANSFER_SIZE_8

1 bytes transfer size


sl_dma_transfer_inc_t#

sl_dma_transfer_inc_t

Enumeration holds DMA transfer address increment for source and destination.

Enumerator
SL_TRANSFER_SRC_INC_32

4 bytes source address increment

SL_TRANSFER_SRC_INC_16

2 bytes source address increment

SL_TRANSFER_SRC_INC_8

1 byte source address increment

SL_TRANSFER_SRC_INC_NONE

No source address increment.

SL_TRANSFER_DST_INC_32

4 bytes destination address increment

SL_TRANSFER_DST_INC_16

2 bytes destination address increment

SL_TRANSFER_DST_INC_8

1 byte destination address increment

SL_TRANSFER_DST_INC_NONE

No destination address increment.


sl_dma_callback_code_t#

sl_dma_callback_code_t

Enumeration holds 8-bit codes which are used by callback_type in sl_si91x_dma_unregister_callbacks function.

Enumerator
SL_DMA_TRANSFER_DONE_CB

8-bit code for transfer complete callback

SL_DMA_ERROR_CB

8-bit code for error callback


Typedef Documentation#

sl_dma_transfer_complete#

typedef void(* sl_dma_transfer_complete) (uint32_t channel, void *data) )(uint32_t channel, void *data)

Typedef for user supplied callback function which is called when a DMA transfer completes.

Parameters
TypeDirectionArgument NameDescription
[in]channel_no

DMA channel number

[in]*data

An extra parameter for user application


sl_dma_error#

typedef void(* sl_dma_error) (uint32_t channel, void *data) )(uint32_t channel, void *data)

Typedef for user supplied callback function which is called when a DMA error occurs.

Parameters
TypeDirectionArgument NameDescription
[in]channel_no

DMA channel number

[in]*data

An extra parameter for user application


Variable Documentation#

sl_channel_allocation_data_t#

sl_channel_data_t sl_channel_allocation_data_t[2][SL_CHANNEL_COUNT]

DMA driver channel allocator.


Function Documentation#

sl_si91x_dma_init#

sl_status_t sl_si91x_dma_init (sl_dma_init_t * dma_init)

Initialize DMA peripheral by enabling DMA clock and clearing DMA interrupts.

Parameters
TypeDirectionArgument NameDescription
sl_dma_init_t *[in]dma_init

dma initialization structure, dma_init->dma_number - 0->UDMA0, 1->UDMA1 dma_init->dma_channel_count - Number of channels used by DMA driver (0-32)

Returns

  • Initialization status SL_STATUS_OK - Initialization success SL_STATUS_NOT_INITIALIZED - Initialization fail


sl_si91x_dma_deinit#

sl_status_t sl_si91x_dma_deinit (uint32_t dma_number)

Deinitialize the DMA module by disabling peripheral clock and interrupts, if there is no ongoing DMA transfer.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]dma_number

0->UDMA0, 1->UDMA1

Returns

  • deinitialization status SL_STATUS_OK - Deinit success SL_STATUS_BUSY - Cannot deinit the peripheral due to an ongoing transfer SL_STATUS_NOT_INITIALIZED - DMA peripheral not initialized


sl_si91x_dma_allocate_channel#

sl_status_t sl_si91x_dma_allocate_channel (uint32_t dma_number, uint32_t * channel_no, uint32_t priority)

Check the available DMA channel and allocate the channel.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]dma_number

dma_number 0->UDMA0, 1->UDMA1

uint32_t *[in]channel_no

Address of channel number.

uint32_t[in]priority

channel priority.

This function also sets the priority of allocated channel and assign the channel number to *channel_no variable. If no channel is available, it will return SL_DMA_NO_CHANNEL_AVAILABLE. note: Users can also initialize the desired channel number and this API checks whether the desired channel is available and allocates the channel if available. To allocate the available channel, channel_no should be initialized to 0.

  • This function should be called after initializing DMA using sl_si91x_dma_init

Returns

  • channel allocation status SL_STATUS_OK - Channel allocated SL_STATUS_DMA_NO_CHANNEL_AVAILABLE - All DMA channels are allocated SL_STATUS_DMA_CHANNEL_ALLOCATED - Desired channel is already allocated SL_STATUS_NOT_INITIALIZED - DMA peripheral not initialized SL_STATUS_INVALID_PARAMETER - Channel no is invalid


sl_si91x_dma_deallocate_channel#

sl_status_t sl_si91x_dma_deallocate_channel (uint32_t dma_number, uint32_t channel_no)

Deallocate the DMA channel if there is no ongoing transfer on channel.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]dma_number

dma_number 0->UDMA0, 1->UDMA1

uint32_t[in]channel_no

channel number.

Returns

  • channel deallocation status SL_STATUS_OK - Channel deallocated SL_STATUS_BUSY - Cannot deallocate channel due to an ongoing transfer SL_STATUS_NOT_INITIALIZED - DMA peripheral not initialized SL_STATUS_INVALID_PARAMETER - Channel no is invalid


sl_si91x_dma_register_callbacks#

sl_status_t sl_si91x_dma_register_callbacks (uint32_t dma_number, uint32_t channel_no, sl_dma_callback_t * callback_t)

Register DMA callbacks (transfer complete & error).

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]dma_number

dma_number 0->UDMA0, 1->UDMA1

uint32_t[in]channel_no

channel number.

sl_dma_callback_t *[in]callback_t

structure containing callback functions.

Users must update the sl_dma_callback_t structure and pass its address to this function. Users can have separate callbacks for transfer complete and error for each channel.

  • This function should be called after sl_si91x_dma_init and sl_si91x_dma_allocate_channel

Returns

  • channel deallocation status SL_STATUS_OK - Callback registered successfully SL_STATUS_INVALID_PARAMETER - Invalid channel number SL_STATUS_NOT_INITIALIZED - DMA peripheral not initialized


sl_si91x_dma_unregister_callbacks#

sl_status_t sl_si91x_dma_unregister_callbacks (uint32_t dma_number, uint32_t channel_no, uint8_t callback_type)

Unregister DMA callbacks (transfer complete & error).

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]dma_number

dma_number 0->UDMA0, 1->UDMA1

uint32_t[in]channel_no

channel number.

uint8_t[in]callback_type

Unregister the DMA callbacks based on the callback type (bit mapped to callbacks), (SL_DMA_TRANSFER_DONE_CB) - unregister transfer complete callback (SL_DMA_ERROR_CB) - unregister error callback (SL_DMA_TRANSFER_DONE_CB | SL_DMA_ERROR_CB) - unregister both transfer complete and error callback

Update the 8-bit variable callback_type and pass to the function. Each bit is mapped to a specific callback.

Returns

  • channel deallocation status SL_STATUS_OK - Callback unregistered successfully SL_STATUS_INVALID_PARAMETER - Invalid channel number SL_STATUS_NOT_INITIALIZED - DMA peripheral not initialized


sl_si91x_dma_transfer#

sl_status_t sl_si91x_dma_transfer (uint32_t dma_number, uint32_t channel_no, sl_dma_xfer_t * dma_transfer_t)

Configure the DMA channel descriptor and initiate DMA transfer.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]dma_number

dma_number 0->UDMA0, 1->UDMA1

uint32_t[in]channel_no

channel number.

sl_dma_xfer_t *[in]dma_transfer_t

channel transfer data structure containing channel descriptor and other basic DMA parameters.

DMA primary descriptor is updated in this function and based on transfer mode the alternate descriptor is also updated (only for ping pong mode). Additionally, other DMA parameters such as peripheral ACK signal (for peripheral memory transfers), DMA priority etc. are also updated.

  • This function should be called after sl_si91x_dma_init and sl_si91x_dma_allocate_channel

Returns

  • DMA transfer status SL_STATUS_OK - Transfer started successfully SL_STATUS_SUSPENDED - Transfer initialization fail SL_STATUS_NOT_INITIALIZED - DMA peripheral not initialized SL_STATUS_INVALID_PARAMETER - Channel no is invalid


sl_si91x_dma_simple_transfer#

sl_status_t sl_si91x_dma_simple_transfer (uint32_t dma_number, uint32_t channel_no, void * src_addr, void * dst_addr, uint32_t data_size)

Configure the DMA channel descriptor and initiate simple memory to memory DMA transfer.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]dma_number

dma_number 0->UDMA0, 1->UDMA1

uint32_t[in]channel_no

channel no

void *[in]src_addr

source address.

void *[in]dst_addr

destination address.

uint32_t[in]data_size

transfer size in bytes

Pass the source address and destination address of transfer along with transfer length in bytes.

  • This function should be called after sl_si91x_dma_init and sl_si91x_dma_allocate_channel

Returns

  • DMA transfer status SL_STATUS_OK - Transfer success SL_STATUS_SUSPENDED - Transfer initialization fail SL_STATUS_NOT_INITIALIZED - DMA peripheral not initialized SL_STATUS_INVALID_PARAMETER - Channel no is invalid


sl_si91x_dma_stop_transfer#

sl_status_t sl_si91x_dma_stop_transfer (uint32_t dma_number, uint32_t channel_no)

Stop any active transfer on a channel.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]dma_number

dma_number 0->UDMA0, 1->UDMA1

uint32_t[in]channel_no

channel number.

If there is no active transfer on the channel, this function returns SL_DMA_CHANNEL_IDLE.

  • This function should be called after sl_si91x_dma_init and sl_si91x_dma_allocate_channel

Returns

  • DMA transfer status SL_STATUS_OK - Transfer stopped successfully SL_STATUS_IDLE - There is no active transfer on channel SL_STATUS_INVALID_PARAMETER - Invalid channel number SL_STATUS_NOT_INITIALIZED - DMA peripheral not initialized


sl_si91x_dma_channel_status_get#

sl_status_t sl_si91x_dma_channel_status_get (uint32_t dma_number, uint32_t channel_no)

Return the channel status i.e., whether the channel is allocated/busy/idle.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]dma_number

dma_number 0->UDMA0, 1->UDMA1

uint32_t[in]channel_no

channel number.

  • This function should be called after sl_si91x_dma_init

Returns

  • channel status SL_STATUS_IDLE - Channel is not allocated SL_STATUS_DMA_CHANNEL_ALREADY_ALLOCATED - Channel is already allocated and idle SL_STATUS_BUSY - Channel is allocated and busy SL_STATUS_NOT_INITIALIZED - DMA peripheral not initialized SL_STATUS_INVALID_PARAMETER - Channel no is invalid