Network Interface#

Functions#

sl_status_t
sl_net_init(sl_net_interface_t interface, const void *configuration, void *context, sl_net_event_handler_t event_handler)

Initialize a network interface.

sl_status_t
sl_net_deinit(sl_net_interface_t interface, void *context)

De-initialize a network interface.

sl_status_t
sl_net_up(sl_net_interface_t interface, sl_net_profile_id_t profile_id)

Bring a network interface up.

sl_status_t
sl_net_down(sl_net_interface_t interface)

Bring a network interface down.

sl_status_t
sl_dns_host_get_by_name(const char *host_name, const uint32_t timeout, const sl_net_dns_resolution_ip_type_t dns_resolution_ip, sl_ip_address_t *ip_address)

Resolve given host name to IP address.

Function Documentation#

sl_net_init#

sl_status_t sl_net_init (sl_net_interface_t interface, const void * configuration, void * context, sl_net_event_handler_t event_handler)

Initialize a network interface.

Parameters
[in]interface

Interface identified by sl_net_interface_t

[in]configuration

Configuration object specific to network interface.

[in]context

Runtime context specific to network interface.

[in]event_handler

Processes all events related to network interface.

This API should be called before calling any sl_net API. Returns


Definition at line 54 of file components/service/network_manager/inc/sl_net.h

sl_net_deinit#

sl_status_t sl_net_deinit (sl_net_interface_t interface, void * context)

De-initialize a network interface.

Parameters
[in]interface

Interface identified by sl_net_interface_t

[in]context

Runtime context specific to network interface.

Returns


Definition at line 73 of file components/service/network_manager/inc/sl_net.h

sl_net_up#

sl_status_t sl_net_up (sl_net_interface_t interface, sl_net_profile_id_t profile_id)

Bring a network interface up.

Parameters
[in]interface

Interface identified by sl_net_interface_t

[in]profile_id

SL Network profile identifier for specific interface.

Returns


Definition at line 87 of file components/service/network_manager/inc/sl_net.h

sl_net_down#

sl_status_t sl_net_down (sl_net_interface_t interface)

Bring a network interface down.

Parameters
[in]interface

Interface identified by sl_net_interface_t

Returns


Definition at line 99 of file components/service/network_manager/inc/sl_net.h

sl_dns_host_get_by_name#

sl_status_t sl_dns_host_get_by_name (const char * host_name, const uint32_t timeout, const sl_net_dns_resolution_ip_type_t dns_resolution_ip, sl_ip_address_t * ip_address)

Resolve given host name to IP address.

Parameters
N/Ahost_name

Host name which needs to be resolved.

N/Atimeout

If value is greater than zero, caller would be blocked till timeout milliseconds to get the response. If the values is equal's to zero, response would sent asynchronously using callbacks.

N/Adns_resolution_ip

Whether the host name needs to be resolved to IPV4 or IPV6.

N/Aip_address

IP address object to store resolved IP address

Returns


Definition at line 38 of file components/service/network_manager/inc/sl_net_dns.h