Public Attributes#
uint8_t
Address type of the connected device.
uint8_t
Address of the connected device.
uint8_t
status of the connection - success/failure
Public Attribute Documentation#
dev_addr_type#
uint8_t rsi_ble_event_conn_status_s::dev_addr_type
Address type of the connected device.
Definition at line
89
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
dev_addr#
uint8_t rsi_ble_event_conn_status_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the connected device.
Definition at line
91
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
status#
uint8_t rsi_ble_event_conn_status_s::status
status of the connection - success/failure
Definition at line
93
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h