Public Attributes#

uint8_t

remote device address

uint8_t

attribute handle

uint8_t

length of attribute value

uint8_t

This contains the attribute value.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_event_indication_s::dev_addr[RSI_DEV_ADDR_LEN]

remote device address


Definition at line 843 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

handle#

uint8_t rsi_ble_event_indication_s::handle[2]

attribute handle


Definition at line 845 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

length#

uint8_t rsi_ble_event_indication_s::length

length of attribute value


Definition at line 847 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

att_value#

uint8_t rsi_ble_event_indication_s::att_value[RSI_DEV_ATT_LEN]

This contains the attribute value.

The maximum value is 240, see RSI_DEV_ATT_LEN Macro


Definition at line 849 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h