Public Attributes#
uint16_t, ScanInterval, It is the Time interval from when the Controller started its last scan until it begins the subsequent scan on the primary advertising physical channel.
uint16_t, Scan Window parameter is a recommendation from the host on how long the controller should scan.
uint16_t, Connection interval minimum parameter defines the minimum allowed connection interval.
uint16_t, Connection interval maximum parameter defines the maximum allowed connection interval.
uint16_t, Connection Latency or Maximum Latency parameter defines the maximum allowed Peripheral latency.
uint16_t,Connection Timeout or Supervision Timeout parameter defines the link supervision timeout for the connection.
uint16_t,The Min CE Length parameter provide the Controller with the expected minimum length of the connection events.
uint16_t,The Max CE Length parameter provide the controller with the expected maximum length of the connection events.
Public Attribute Documentation#
ScanInterval#
uint16_t rsi_ble_initiation_params_s::ScanInterval
uint16_t, ScanInterval, It is the Time interval from when the Controller started its last scan until it begins the subsequent scan on the primary advertising physical channel.
Range : 0x0004 to 0xFFFF
1497
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
ScanWindow#
uint16_t rsi_ble_initiation_params_s::ScanWindow
uint16_t, Scan Window parameter is a recommendation from the host on how long the controller should scan.
Range : 0x0004 to 0xFFFF
1500
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
ConnIntervalMin#
uint16_t rsi_ble_initiation_params_s::ConnIntervalMin
uint16_t, Connection interval minimum parameter defines the minimum allowed connection interval.
Range: 0x0006 to 0x0C80
1503
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
ConnIntervalMax#
uint16_t rsi_ble_initiation_params_s::ConnIntervalMax
uint16_t, Connection interval maximum parameter defines the maximum allowed connection interval.
Range: 0x0006 to 0x0C80
1506
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
ConnLatency#
uint16_t rsi_ble_initiation_params_s::ConnLatency
uint16_t, Connection Latency or Maximum Latency parameter defines the maximum allowed Peripheral latency.
Range: 0x0000 to 0x01F3
1509
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
ConnSTO#
uint16_t rsi_ble_initiation_params_s::ConnSTO
uint16_t,Connection Timeout or Supervision Timeout parameter defines the link supervision timeout for the connection.
Range: 0x000A to 0x0C80
1512
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
MinCELen#
uint16_t rsi_ble_initiation_params_s::MinCELen
uint16_t,The Min CE Length parameter provide the Controller with the expected minimum length of the connection events.
Range: 0x0000 to 0xFFFF
1515
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
MaxCELen#
uint16_t rsi_ble_initiation_params_s::MaxCELen
uint16_t,The Max CE Length parameter provide the controller with the expected maximum length of the connection events.
Range: 0x0000 to 0xFFFF
1518
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h