Functionality Breaks between SDK v2.x and v3.x#

The following are the features in WiSeConnect™ SDK v2.x that are not supported in v3.x:

  • Synchronous scanning of Wi-Fi Service Set Identifiers (SSIDs) - the SDK supports asynchronous scanning.

  • Bare Metal applications - applications must run on the Real-Time Operating System (RTOS).

  • File Transfer Protocol (FTP)

  • Compiling applications with STM35™ and RT595™ processors as external hosts.

  • AT mode command interface over UART and USB