Wi-Fi advanced scan configuration options.
Public Attributes#
RSSI level to trigger advanced scan.
RSSI level to trigger advanced scan.
Time spent on each channel when performing active scan (milliseconds).
Time spent on each channel when performing passive scan (milliseconds).
Flag to start advanced scan immediately.
Flag to indicate to send multiple probes to AP. If set. a probe request would be sent to all access points in addition to connected SSID.
Public Attribute Documentation#
trigger_level#
int32_t sl_wifi_advanced_scan_configuration_t::trigger_level
RSSI level to trigger advanced scan.
143
of file components/protocol/wifi/inc/sl_wifi_types.h
trigger_level_change#
uint32_t sl_wifi_advanced_scan_configuration_t::trigger_level_change
RSSI level to trigger advanced scan.
144
of file components/protocol/wifi/inc/sl_wifi_types.h
active_channel_time#
uint16_t sl_wifi_advanced_scan_configuration_t::active_channel_time
Time spent on each channel when performing active scan (milliseconds).
145
of file components/protocol/wifi/inc/sl_wifi_types.h
passive_channel_time#
uint16_t sl_wifi_advanced_scan_configuration_t::passive_channel_time
Time spent on each channel when performing passive scan (milliseconds).
146
of file components/protocol/wifi/inc/sl_wifi_types.h
enable_instant_scan#
uint8_t sl_wifi_advanced_scan_configuration_t::enable_instant_scan
Flag to start advanced scan immediately.
147
of file components/protocol/wifi/inc/sl_wifi_types.h
enable_multi_probe#
uint8_t sl_wifi_advanced_scan_configuration_t::enable_multi_probe
Flag to indicate to send multiple probes to AP. If set. a probe request would be sent to all access points in addition to connected SSID.
149
of file components/protocol/wifi/inc/sl_wifi_types.h