Wi-Fi firmware version information.

Public Attributes#

uint8_t

Chip ID.

uint8_t

ROM ID.

uint8_t

Major version number.

uint8_t

Minor version number.

uint8_t

Security enabled or disabled.

uint8_t

Patch number.

uint8_t

Customer ID.

uint16_t

Build number.

Public Attribute Documentation#

chip_id#

uint8_t sl_wifi_firmware_version_t::chip_id

Chip ID.


Definition at line 105 of file components/protocol/wifi/inc/sl_wifi_types.h

rom_id#

uint8_t sl_wifi_firmware_version_t::rom_id

ROM ID.


Definition at line 106 of file components/protocol/wifi/inc/sl_wifi_types.h

major#

uint8_t sl_wifi_firmware_version_t::major

Major version number.


Definition at line 107 of file components/protocol/wifi/inc/sl_wifi_types.h

minor#

uint8_t sl_wifi_firmware_version_t::minor

Minor version number.


Definition at line 108 of file components/protocol/wifi/inc/sl_wifi_types.h

security_version#

uint8_t sl_wifi_firmware_version_t::security_version

Security enabled or disabled.


Definition at line 109 of file components/protocol/wifi/inc/sl_wifi_types.h

patch_num#

uint8_t sl_wifi_firmware_version_t::patch_num

Patch number.


Definition at line 110 of file components/protocol/wifi/inc/sl_wifi_types.h

customer_id#

uint8_t sl_wifi_firmware_version_t::customer_id

Customer ID.


Definition at line 111 of file components/protocol/wifi/inc/sl_wifi_types.h

build_num#

uint16_t sl_wifi_firmware_version_t::build_num

Build number.


Definition at line 112 of file components/protocol/wifi/inc/sl_wifi_types.h