TWT reschedule structure.

Public Attributes#

uint8_t

TWT session flow id.

uint16_t

Reserved.

uint8_t

Reserved.

uint64_t

Duration to suspend respective TWT session.

Public Attribute Documentation#

flow_id#

uint8_t sl_wifi_reschedule_twt_config_t::flow_id

TWT session flow id.


Definition at line 317 of file components/protocol/wifi/inc/sl_wifi_types.h

twt_action#

sl_wifi_reschedule_twt_action_t sl_wifi_reschedule_twt_config_t::twt_action

Suspension time for TWT.


Definition at line 318 of file components/protocol/wifi/inc/sl_wifi_types.h

reserved1#

uint16_t sl_wifi_reschedule_twt_config_t::reserved1

Reserved.


Definition at line 319 of file components/protocol/wifi/inc/sl_wifi_types.h

reserved2#

uint8_t sl_wifi_reschedule_twt_config_t::reserved2

Reserved.


Definition at line 320 of file components/protocol/wifi/inc/sl_wifi_types.h

suspend_duration#

uint64_t sl_wifi_reschedule_twt_config_t::suspend_duration

Duration to suspend respective TWT session.


Definition at line 321 of file components/protocol/wifi/inc/sl_wifi_types.h