Queue Management#
WiSeConnectâ„¢ SDK v3.x has a total of 12 queues:
5 for sending commands to the network processor, such as a command to scan for access points (APs).
5 for processing command responses from the network processor.
2 for asynchronous processing such as the handling of asynchronous command responses.
WiSeConnect SDK v2.x has 6 queues:
1 for sending commands.
5 that are shared for the purpose of processing command responses, as well as asynchronous processing.