HTTP read data parameters.
Public Attributes#
Pointer to request structure received in the request handler.
uint8_t *
Pointer to user defined memory buffer.
uint32_t
Length of user defined memory buffer given.
uint32_t
Amount of data received in the read operation.
Public Attribute Documentation#
request#
sl_http_server_request_t* sl_http_recv_req_data_t::request
Pointer to request structure received in the request handler.
buffer_length#
uint32_t sl_http_recv_req_data_t::buffer_length
Length of user defined memory buffer given.
received_data_length#
uint32_t sl_http_recv_req_data_t::received_data_length
Amount of data received in the read operation.