HTTP server request parameters.
Public Attributes#
URI of the request.
HTTP protocol version.
uint16_t
Number of request headers received.
Type of the request (GET, POST, etc.)
uint32_t
Length of the request data.
Public Attribute Documentation#
request_header_count#
uint16_t sl_http_server_request_s::request_header_count
Number of request headers received.
type#
sl_http_server_request_type_t sl_http_server_request_s::type
Type of the request (GET, POST, etc.)
request_data_length#
uint32_t sl_http_server_request_s::request_data_length
Length of the request data.