Public Attributes#

uint8_t

type - Specifies whether to remove or clear the advertising sets.

uint8_t

uint8_t Advertising_Handle, used to identify Advertising set, Ranges from 0x00 to 0xEF

Public Attribute Documentation#

type#

uint8_t rsi_ble_ae_adv_set_clear_or_remove_s::type

type - Specifies whether to remove or clear the advertising sets.

{1} - clear {2} - remove


Definition at line 1318 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

adv_handle#

uint8_t rsi_ble_ae_adv_set_clear_or_remove_s::adv_handle

uint8_t Advertising_Handle, used to identify Advertising set, Ranges from 0x00 to 0xEF


Definition at line 1320 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h