Public Attributes#

uint8_t

uint8_t Advertising_Handle, Used to identify an advertising set , Range : 0x00 to 0xEF

uint8_t

uint8[6] Random_Address , The Random Address may be of either Static Address or Private Address

Public Attribute Documentation#

adv_handle#

uint8_t rsi_ble_ae_set_random_address_s::adv_handle

uint8_t Advertising_Handle, Used to identify an advertising set , Range : 0x00 to 0xEF


Definition at line 1167 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

addr#

uint8_t rsi_ble_ae_set_random_address_s::addr[RSI_DEV_ADDR_LEN]

uint8[6] Random_Address , The Random Address may be of either Static Address or Private Address


Definition at line 1169 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h