Public Attributes#

uint8_t

uint8_t, Type Type Values Description 1 Adding Device to Periodic Advertising list 2 Removing Device from Periodic Advertising list 3 Clearing Periodic Advertising List

uint8_t

uint8_t, Advertiser Address Type, this parameter indicates the type of address being used in the connection request packets

uint8_t

uint8_t, Advertiser Address[6]

uint8_t

uint8_t, Advertising_Sid, Value of the Advertising SID subfield in the ADI field of the PDU, Range : 0x00 to 0x0F

Public Attribute Documentation#

type#

uint8_t rsi_ble_ae_dev_to_periodic_list_s::type

uint8_t, Type Type Values Description 1 Adding Device to Periodic Advertising list 2 Removing Device from Periodic Advertising list 3 Clearing Periodic Advertising List


Definition at line 1494 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

adv_addr_type#

uint8_t rsi_ble_ae_dev_to_periodic_list_s::adv_addr_type

uint8_t, Advertiser Address Type, this parameter indicates the type of address being used in the connection request packets

      0x00          Public Device Address or Public Identity Address
      0x01          Random Device Address or Random (static) Identity Address

All other values Reserved for future use


Definition at line 1501 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

adv_addr#

uint8_t rsi_ble_ae_dev_to_periodic_list_s::adv_addr[RSI_DEV_ADDR_LEN]

uint8_t, Advertiser Address[6]


Definition at line 1503 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

adv_sid#

uint8_t rsi_ble_ae_dev_to_periodic_list_s::adv_sid

uint8_t, Advertising_Sid, Value of the Advertising SID subfield in the ADI field of the PDU, Range : 0x00 to 0x0F


Definition at line 1505 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h