Structure to hold the parameters of Analog comparator configurations.

Public Attributes#

uint8_t

comparator number, sl_analog_comparator_number_t for possible values

uint8_t

comparator non inverting input, sl_analog_comparator_inputs_t for possible values

uint8_t

comparator non inverting input, sl_analog_comparator_inputs_t for possible values

uint8_t
boolean_t

true to enable and false to disable filter for comparator

Public Attribute Documentation#

comparator_number#

uint8_t sl_analog_comparator_config_t::comparator_number

comparator number, sl_analog_comparator_number_t for possible values


Definition at line 185 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h

non_inverting_input#

uint8_t sl_analog_comparator_config_t::non_inverting_input

comparator non inverting input, sl_analog_comparator_inputs_t for possible values


Definition at line 187 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h

inverting_input#

uint8_t sl_analog_comparator_config_t::inverting_input

comparator non inverting input, sl_analog_comparator_inputs_t for possible values


Definition at line 188 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h

hystersis_value#

uint8_t sl_analog_comparator_config_t::hystersis_value

comparator hystersis control value sl_analog_comparator_hystersis_values_t


Definition at line 189 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h

is_filter_enabled#

boolean_t sl_analog_comparator_config_t::is_filter_enabled

true to enable and false to disable filter for comparator


Definition at line 190 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h