Structure to hold the clock configuration parameters.
Public Attributes#
uint8_t
SoC PLL count value.
uint16_t
Int PLL control value.
uint32_t
Intf PLL clock frequency.
uint32_t
Intf PLL reference clock frequency.
uint32_t
SoC PLL clock frequency.
uint32_t
SoC PLL reference clock frequency.
uint16_t
Clock Division Factor.
Public Attribute Documentation#
soc_pll_mm_count_value#
uint8_t sl_gspi_clock_config_t::soc_pll_mm_count_value
SoC PLL count value.
Definition at line
117
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h
intf_pll_500_control_value#
uint16_t sl_gspi_clock_config_t::intf_pll_500_control_value
Int PLL control value.
Definition at line
118
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h
intf_pll_clock#
uint32_t sl_gspi_clock_config_t::intf_pll_clock
Intf PLL clock frequency.
Definition at line
119
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h
intf_pll_reference_clock#
uint32_t sl_gspi_clock_config_t::intf_pll_reference_clock
Intf PLL reference clock frequency.
Definition at line
120
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h
soc_pll_clock#
uint32_t sl_gspi_clock_config_t::soc_pll_clock
SoC PLL clock frequency.
Definition at line
121
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h
soc_pll_reference_clock#
uint32_t sl_gspi_clock_config_t::soc_pll_reference_clock
SoC PLL reference clock frequency.
Definition at line
122
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h
division_factor#
uint16_t sl_gspi_clock_config_t::division_factor
Clock Division Factor.
Definition at line
123
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_gspi.h