Structure to hold the parameters of the SYSRTC clock-source configurations.
Public Attribute Documentation#
clock_source#
uint8_t sl_sysrtc_clock_config_t::clock_source
input clock sources \refsl_clock_sources_t
Definition at line
85
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h
division_factor#
uint32_t sl_sysrtc_clock_config_t::division_factor
clock division factor
Definition at line
86
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sysrtc.h