Structure to hold the parameters of timer configurations.

Public Attributes#

uint8_t

timer number, SL_ULP_TIMER_NUMBER for default values

uint8_t

timer mode, SL_ULP_TIMER_MODE for default values

uint8_t

timer type, SL_ULP_TIMER_TYPE for default values

uint32_t

timer match value SL_ULP_TIMER_MATCH_VALUE(delay time) in microseconds

uint8_t

timer direction, SL_ULP_TIMER_DIRECTION for default values

Public Attribute Documentation#

timer_num#

uint8_t ulp_timer_config_t::timer_num

timer number, SL_ULP_TIMER_NUMBER for default values


Definition at line 113 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ulp_timer.h

timer_mode#

uint8_t ulp_timer_config_t::timer_mode

timer mode, SL_ULP_TIMER_MODE for default values


Definition at line 114 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ulp_timer.h

timer_type#

uint8_t ulp_timer_config_t::timer_type

timer type, SL_ULP_TIMER_TYPE for default values


Definition at line 115 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ulp_timer.h

timer_match_value#

uint32_t ulp_timer_config_t::timer_match_value

timer match value SL_ULP_TIMER_MATCH_VALUE(delay time) in microseconds


Definition at line 116 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ulp_timer.h

timer_direction#

uint8_t ulp_timer_config_t::timer_direction

timer direction, SL_ULP_TIMER_DIRECTION for default values


Definition at line 117 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_ulp_timer.h