Structure to hold the parameters of watchdog timer clock-source configurations.
Public Attributes#
uint8_t
low frequency FSM clock source, low_freq_fsm_clock_t
uint8_t
high frequency FSM clock source, high_freq_fsm_clock_t
uint8_t
bg_pmu clock source, bg_pmu_clock_t
Public Attribute Documentation#
low_freq_fsm_clock_src#
uint8_t watchdog_timer_clock_config_t::low_freq_fsm_clock_src
low frequency FSM clock source, low_freq_fsm_clock_t
Definition at line
109
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_watchdog_timer.h
high_freq_fsm_clock_src#
uint8_t watchdog_timer_clock_config_t::high_freq_fsm_clock_src
high frequency FSM clock source, high_freq_fsm_clock_t
Definition at line
110
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_watchdog_timer.h
bg_pmu_clock_source#
uint8_t watchdog_timer_clock_config_t::bg_pmu_clock_source
bg_pmu clock source, bg_pmu_clock_t
Definition at line
111
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_watchdog_timer.h