Functions#
This section provides a reference to the Crypto utility API functions used for AES.
Functions#
To perform PKCS #7 padding on the given data.
To unpad a PKCS #7 padded data array in-place, and return the length of the unpadded data.
Function Documentation#
pkcs7_padding#
uint8_t * pkcs7_padding (uint8_t * data, size_t data_length, size_t block_size, size_t * padded_data_length)
To perform PKCS #7 padding on the given data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | data | Pointer to the data to be padded. |
| size_t | [in] | data_length | Length of the data in bytes. |
| size_t | [in] | block_size | Size of the block in bytes (typically 16 for AES). |
| size_t * | [out] | padded_data_length |
|
Returns
Returns a pointer to the padded data.
pkcs7_unpad#
int pkcs7_unpad (unsigned char * data, size_t data_length)
To unpad a PKCS #7 padded data array in-place, and return the length of the unpadded data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| unsigned char * | [in] | data | Pointer to the data array containing PKCS #7 padded data. |
| size_t | [in] | data_length | Length of the data array. |
This function performs PKCS #7 unpadding on the input data array. It checks the padding bytes at the end of the array, removes them if they are valid, and returns the length of the unpadded data.
Returns
The length of the unpadded data, or -1, if the padding is invalid or data is empty.