SNTP client configuration structure.
This structure holds the configuration parameters for the SNTP client, including server details, synchronization methods, timeouts, and various flags.
Public Attributes#
SNTP server host name or address.
SNTP method. One of the defines from SNTP Methods.
SNTP operation timeout in milliseconds (ms).
SNTP flags.
SNTP response handler of type sl_sntp_client_event_handler_t.
Time synchronization notification handler of type sl_sntp_set_time_sync_notification_handler_t.
Set to true if smooth synchronization is required.
Set to true to request NTP server configuration from DHCP.
Set to true to refresh the server list if NTP is provided by DHCP.
Public Attribute Documentation#
server_host_name#
uint8_t* sl_sntp_client_config_t::server_host_name
SNTP server host name or address.
sntp_method#
uint8_t sl_sntp_client_config_t::sntp_method
SNTP method. One of the defines from SNTP Methods.
sntp_timeout#
uint16_t sl_sntp_client_config_t::sntp_timeout
SNTP operation timeout in milliseconds (ms).
flags#
uint8_t sl_sntp_client_config_t::flags
SNTP flags.
Combination of values from SNTP Flags. Note
- Bits 1-7 are reserved. User must set them to 0. 
event_handler#
sl_sntp_client_event_handler_t sl_sntp_client_config_t::event_handler
SNTP response handler of type sl_sntp_client_event_handler_t.
time_sync_notifiication_handler#
sl_sntp_set_time_sync_notification_handler_t sl_sntp_client_config_t::time_sync_notifiication_handler
Time synchronization notification handler of type sl_sntp_set_time_sync_notification_handler_t.
Note
- This feature is currently not supported in Si917 chipsets. 
smooth_sync#
bool sl_sntp_client_config_t::smooth_sync
Set to true if smooth synchronization is required.
Note
- This feature is currently not supported in Si917 chipsets. 
server_from_dhcp#
bool sl_sntp_client_config_t::server_from_dhcp
Set to true to request NTP server configuration from DHCP.
Note
- This feature is currently not supported in Si917 chipsets. 
renew_servers_after_new_ip#
bool sl_sntp_client_config_t::renew_servers_after_new_ip
Set to true to refresh the server list if NTP is provided by DHCP.
Note
- This feature is currently not supported in Si917 chipsets.