Folder Structure#
This section outlines the folder structure of the WiSeConnectâ„¢ SDK v3.x GitHub repository.
Folder | Description |
|---|---|
| WiSeConnect 3.x source code and Simplicity Studio component definitions |
| Network processor firmware images (organized into subfolders) |
| Lite firmware image |
| Standard firmware image |
| Documentation (including release notes, software reference manual, and app notes) |
| Application examples |
| Resources (organized into subfolders) |
| Certificates |
| Simplicity Studio component definition for certificates |
| Default configuration header files |
| Default configurations for the Lightweight IP (LwIP) networking layers used in hosted mode |
| Miscellaneous declarations and configuration settings |
| Example scripts (including Python test scripts) |
| Third-party software, such as Amazon web services internet-of-things (AWS IoT) SDK, Azure SDK, and others |
| Common utility functions for internet protocol version 6 (IPv6), logging, certificate handling, and others |