Structure representing the BLE Advertising Extensions (AE) command to read the supported maximum advertising data.
This structure is used to define the parameters for a BLE AE command to read the supported maximum advertising data, including a reserved field for future use or alignment.
Public Attributes#
uint16_t
Reserved field for future use or alignment.
Public Attribute Documentation#
reserved#
uint16_t rsi_ble_ae_read_supported_max_adv_data_s::reserved
Reserved field for future use or alignment.
Definition at line 1795
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h