You are viewing documentation for version:
3.3.3
Structure representing the BLE connection request.
This structure is used to define the parameters for a BLE connection request, including the address type and address of the device to connect, scan interval, scan window, connection interval, connection latency, and supervision timeout.
Public Attributes# uint8_t
Address type of the device to connect.
uint8_t
Address of the device to connect.
uint16_t
Minimum connection interval.
uint16_t
Maximum connection interval.
Public Attribute Documentation# dev_addr_type# uint8_t rsi_ble_req_conn_s::dev_addr_type Address type of the device to connect.
dev_addr# uint8_t rsi_ble_req_conn_s::dev_addr[RSI_DEV_ADDR_LEN] Address of the device to connect.
le_scan_interval# uint16_t rsi_ble_req_conn_s::le_scan_interval Scan interval.
le_scan_window# uint16_t rsi_ble_req_conn_s::le_scan_window Scan window.
conn_interval_min# uint16_t rsi_ble_req_conn_s::conn_interval_min Minimum connection interval.
conn_interval_max# uint16_t rsi_ble_req_conn_s::conn_interval_max Maximum connection interval.
conn_latency# uint16_t rsi_ble_req_conn_s::conn_latency Connection latency.
supervision_tout# uint16_t rsi_ble_req_conn_s::supervision_tout Supervision timeout.