Structure representing the BLE Advertising Extensions (AE) command to get the supported number of advertising sets.

This structure is used to define the parameters for a BLE AE command to get the supported number of advertising sets, including a reserved field.

Public Attributes#

uint16_t

Reserved field.

Public Attribute Documentation#

reserved#

uint16_t rsi_ble_ae_get_supported_no_of_adv_sets_s::reserved

Reserved field.


Definition at line 1784 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h