Structure to hold the parameters of timer action's AND-event and OR-event configurations.

Public Attributes#

uint8_t
uint8_t

AND-event for counter-0 action, see sl_config_timer_event_t.

uint8_t

OR-event for counter-0 action, see sl_config_timer_event_t.

uint8_t

Valid bits for counter-0 action AND-event, possible values 0 to 16.

uint8_t

Valid bits for counter-0 action OR-event, possible values 0 to 16.

uint8_t

AND-event for counter-1 action, see sl_config_timer_event_t.

uint8_t

OR-event for counter-1 action, see sl_config_timer_event_t.

uint8_t

Valid bits for counter-1 action AND-event, possible values 0 to 16.

uint8_t

Valid bits for counter-1 action OR-event, possible values 0 to 16.

Public Attribute Documentation#

action#

uint8_t sl_config_action_event_t::action

CT action, see sl_config_timer_action_t.


Definition at line 282 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

and_event_counter0#

uint8_t sl_config_action_event_t::and_event_counter0

AND-event for counter-0 action, see sl_config_timer_event_t.


Definition at line 283 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

or_event_counter0#

uint8_t sl_config_action_event_t::or_event_counter0

OR-event for counter-0 action, see sl_config_timer_event_t.


Definition at line 284 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

and_event_valid_bits_counter0#

uint8_t sl_config_action_event_t::and_event_valid_bits_counter0

Valid bits for counter-0 action AND-event, possible values 0 to 16.


Definition at line 285 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

or_event_valid_bits_counter0#

uint8_t sl_config_action_event_t::or_event_valid_bits_counter0

Valid bits for counter-0 action OR-event, possible values 0 to 16.


Definition at line 286 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

and_event_counter1#

uint8_t sl_config_action_event_t::and_event_counter1

AND-event for counter-1 action, see sl_config_timer_event_t.


Definition at line 287 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

or_event_counter1#

uint8_t sl_config_action_event_t::or_event_counter1

OR-event for counter-1 action, see sl_config_timer_event_t.


Definition at line 288 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

and_event_valid_bits_counter1#

uint8_t sl_config_action_event_t::and_event_valid_bits_counter1

Valid bits for counter-1 action AND-event, possible values 0 to 16.


Definition at line 289 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

or_event_valid_bits_counter1#

uint8_t sl_config_action_event_t::or_event_valid_bits_counter1

Valid bits for counter-1 action OR-event, possible values 0 to 16.


Definition at line 290 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h