Structure to hold the parameters of timer Output Compare Unit (OCU) configurations.

Public Attributes#

boolean_t

True to enable OCU output of counter-0, false to disable it.

boolean_t

True to enable OCU DMA support of counter-0, false to disable it.

boolean_t

True to enable OCU 8-bit mode of counter-0, false to disable it.

boolean_t

True to enable counter-0 output sync with other channels, false to disable it.

boolean_t

True to enable OCU output of counter-1, false to disable it.

boolean_t

True to enable OCU DMA support of counter-1, false to disable it.

boolean_t

True to enable OCU 8-bit mode of counter-1, false to disable it.

boolean_t

True to enable counter-1 output sync with other channels, false to disable it.

boolean_t

True to enable counter-0 output toggle high, false to disable it.

boolean_t

True to enable counter-0 output toggle low, false to disable it.

boolean_t

True to enable counter-1 output toggle high, false to disable it.

boolean_t

True to enable counter-1 output toggle low, false to disable it.

Public Attribute Documentation#

is_counter0_ocu_output_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter0_ocu_output_enabled

True to enable OCU output of counter-0, false to disable it.


Definition at line 250 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter0_ocu_dma_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter0_ocu_dma_enabled

True to enable OCU DMA support of counter-0, false to disable it.


Definition at line 251 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter0_ocu_8bit_mode_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter0_ocu_8bit_mode_enabled

True to enable OCU 8-bit mode of counter-0, false to disable it.


Definition at line 252 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter0_ocu_sync_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter0_ocu_sync_enabled

True to enable counter-0 output sync with other channels, false to disable it.


Definition at line 254 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_ocu_output_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter1_ocu_output_enabled

True to enable OCU output of counter-1, false to disable it.


Definition at line 255 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_ocu_dma_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter1_ocu_dma_enabled

True to enable OCU DMA support of counter-1, false to disable it.


Definition at line 256 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_ocu_8bit_mode_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter1_ocu_8bit_mode_enabled

True to enable OCU 8-bit mode of counter-1, false to disable it.


Definition at line 257 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_ocu_sync_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter1_ocu_sync_enabled

True to enable counter-1 output sync with other channels, false to disable it.


Definition at line 259 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter0_toggle_output_high_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter0_toggle_output_high_enabled

True to enable counter-0 output toggle high, false to disable it.


Definition at line 261 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter0_toggle_output_low_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter0_toggle_output_low_enabled

True to enable counter-0 output toggle low, false to disable it.


Definition at line 262 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_toggle_output_high_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter1_toggle_output_high_enabled

True to enable counter-1 output toggle high, false to disable it.


Definition at line 264 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h

is_counter1_toggle_output_low_enabled#

boolean_t sl_config_timer_ocu_config_t::is_counter1_toggle_output_low_enabled

True to enable counter-1 output toggle low, false to disable it.


Definition at line 265 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h