PSRAM configuration handle structure.

Public Attributes#

PSRAMDevType

PSRAM Device enum value.

Device ID struct.

uint32_t

Device Density in bits.

uint32_t

Max frequency for normal read.

uint32_t

Max frequency for fast read.

PSRAMRWType

Read-Write type configuration.

spi_config_t

SPI Config for QSPI interface.

uint16_t

Default burst wrap size.

uint16_t

Toggle Burst Wrap size.

Public Attribute Documentation#

deviceName#

PSRAMDevType sl_psram_info_type_t::deviceName

PSRAM Device enum value.


Definition at line 218 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h

deviceID#

sl_psram_id_type_t sl_psram_info_type_t::deviceID

Device ID struct.


Definition at line 219 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h

devDensity#

uint32_t sl_psram_info_type_t::devDensity

Device Density in bits.


Definition at line 220 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h

normalReadMAXFrequency#

uint32_t sl_psram_info_type_t::normalReadMAXFrequency

Max frequency for normal read.


Definition at line 221 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h

fastReadMAXFrequency#

uint32_t sl_psram_info_type_t::fastReadMAXFrequency

Max frequency for fast read.


Definition at line 222 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h

rwType#

PSRAMRWType sl_psram_info_type_t::rwType

Read-Write type configuration.


Definition at line 223 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h

spi_config#

spi_config_t sl_psram_info_type_t::spi_config

SPI Config for QSPI interface.


Definition at line 224 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h

defaultBurstWrapSize#

uint16_t sl_psram_info_type_t::defaultBurstWrapSize

Default burst wrap size.


Definition at line 225 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h

toggleBurstWrapSize#

uint16_t sl_psram_info_type_t::toggleBurstWrapSize

Toggle Burst Wrap size.


Definition at line 226 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram.h