Structure representing an MQTT Client Message.

This structure holds the information for a message received from or sent to the MQTT broker. It includes details such as the Quality of Service level, packet identifier, and message content.

Public Attributes#

Quality of Service level of the message.

uint16_t

Packet identifier of the received message.

bool

Flag indicating whether the message is retained by the broker.

bool

Flag indicating whether this is a duplicate message.

uint8_t *

Pointer to the topic name. Must not be NULL.

uint16_t

Length of the topic name. It should not exceed 202 bytes that includes NULL termination character.

uint8_t *

Pointer to the message content. Must not be NULL.

uint32_t

Length of the message content.

Public Attribute Documentation#

qos_level#

sl_mqtt_qos_t sl_mqtt_client_message_t::qos_level

Quality of Service level of the message.


packet_identifier#

uint16_t sl_mqtt_client_message_t::packet_identifier

Packet identifier of the received message.


is_retained#

bool sl_mqtt_client_message_t::is_retained

Flag indicating whether the message is retained by the broker.


is_duplicate_message#

bool sl_mqtt_client_message_t::is_duplicate_message

Flag indicating whether this is a duplicate message.


topic#

uint8_t* sl_mqtt_client_message_t::topic

Pointer to the topic name. Must not be NULL.


topic_length#

uint16_t sl_mqtt_client_message_t::topic_length

Length of the topic name. It should not exceed 202 bytes that includes NULL termination character.


content#

uint8_t* sl_mqtt_client_message_t::content

Pointer to the message content. Must not be NULL.


content_length#

uint32_t sl_mqtt_client_message_t::content_length

Length of the message content.