Functions#
This section provides a reference to the Ping API functions.
Functions#
Send an ICMP ping request to a specific IP address.
Function Documentation#
sl_si91x_send_ping#
sl_status_t sl_si91x_send_ping (sl_ip_address_t ip_address, uint16_t ping_packet_size)
Send an ICMP ping request to a specific IP address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_ip_address_t | [in] | ip_address | The destination IP address should be of type sl_ip_address_type_t either IPv4 or IPv6. |
| uint16_t | [in] | ping_packet_size | The ping packet size is defined, with a valid range of [0, 300]. |
This function sends an ICMP ping request to a specific IP address (IPv4 or IPv6) with a user defined ping packet size. It verifies the device’s initialization status and validates the IP address type before sending the request to the specific IP address.
Pre-condition:
sl_net_init should be called before this API.
Returns
sl_status_t - Status of the operation.
SL_STATUS_OK: Operation successful.
SL_STATUS_NOT_INITIALIZED: Device is not initialized.
SL_STATUS_INVALID_PARAMETER: Invalid IP address type.
Note
This is an asynchronous API. The response is recieved via sl_net_event_handler_t with SL_NET_PING_RESPONSE_EVENT as event.